Article [#7229] [ltp] LTP test case setrlimit01 fail in latest kernel 3.5.0

[#7229] [ltp] LTP test case setrlimit01 fail in latest kernel 3.5.0

Submitted By: Vivi Li

Open Date

2012-08-07 04:55:26     Close Date

2012-09-20 03:16:57

Priority:

Medium     Assignee:

Bob Liu

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

ALL     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Not reproducible

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.3-2012_Feb_15

App binary format:

N/A     

Summary: [ltp] LTP test case setrlimit01 fail in latest kernel 3.5.0

Details:

LTP test case setrlimit01 fails in latest kernel 3.5.0.

--

root:/> setrlimit01

setrlimit01    1  TPASS  :  RLNMIT_NOFILE functionality is correctULL pointer access

Deferred Exception context

CURRENT PROCESS:

COMM=setrlimit01 PID=241  CPU=0

TEXT = 0x02b80040-0x02b8b940        DATA = 0x02b8b960-0x02b8ee9c

BSS = 0x02b8ee9c-0x02b93d10  USER-STACK = 0x02ba3f74

return address: [0x02b8556c]; contents of:

0x02b85540:  6ff9  601b  549a  3212  9c01  e0a2  1002  c803

0x02b85550:  1800  9201  9c01  9201  0c42  3298  1005  9073

0x02b85560:  0010  0c42  1805  e0a2  2003  9819 [9a01] 9073

0x02b85570:  0010  0000  3200  3212  50d0  0e3a  1818  4349

ADSP-BF527-0.2 525(MHz CCLK) 131(MHz SCLK) (mpu off)

Linux version 3.5.0-ADI-2012R1-pre-00797-g367b7b2 (test@uclinux63-527-usbdev) (gcc version 4.3.5 (ADI-trunk/svn-5764) ) #255 Fri2

SEQUENCER STATUS:               Not tainted

SEQSTAT: 00002027  IPEND: 0008  IMASK: ffff  SYSCFG: 0006

  EXCAUSE   : 0x27

Double Fault

Kernel OOPS in progress

Deferred Exception context

CURRENT PROCESS:

COMM=setrlimit01 PID=241  CPU=0

TEXT = 0x02b80040-0x02b8b940        DATA = 0x02b8b960-0x02b8ee9c

BSS = 0x02b8ee9c-0x02b93d10  USER-STACK = 0x02ba3f74

return address: [0x00036d3a]; contents of:

0x00036d10:  600e  9851  4348  0c00  1ff2  0c06  1ffa  9a21

0x00036d20:  2ff9  0000  04c3  e14c  0000  014f  e10c  0000

0x00036d30:  3018  3239  3402  0c44  1003 [0001] 2000  e14a

0x00036d40:  0000  e10a  0000  9153  6002  304b  5211  0e08

ADSP-BF527-0.2 525(MHz CCLK) 131(MHz SCLK) (mpu off)

Linux version 3.5.0-ADI-2012R1-pre-00797-g367b7b2 (test@uclinux63-527-usbdev) (gcc version 4.3.5 (ADI-trunk/svn-5764) ) #255 Fri2

SEQUENCER STATUS:               Not tainted

SEQSTAT: 00062021  IPEND: 0028  IMASK: ffff  SYSCFG: 0006

  EXCAUSE   : 0x21

--

It passed in the old kernel with bellow log:

--

root:/> setrlimit01

setrlimit01    1  TPASS  :  RLIMIT_NOFILE functionality is correctNULL pointer access

Deferred Exception context

CURRENT PROCESS:

COMM=setrlimit01 PID=238  CPU=0

TEXT = 0x02b80040-0x02b8b940        DATA = 0x02b8b960-0x02b8ee9c

BSS = 0x02b8ee9c-0x02b93d10  USER-STACK = 0x02ba3f74

return address: [0x02b8556c]; contents of:

0x02b85540:  6ff9  601b  549a  3212  9c01  e0a2  1002  c803

0x02b85550:  1800  9201  9c01  9201  0c42  3298  1005  9073

0x02b85560:  0010  0c42  1805  e0a2  2003  9819 [9a01] 9073

0x02b85570:  0010  0000  3200  3212  50d0  0e3a  1818  4349

ADSP-BF527-0.2 525(MHz CCLK) 131(MHz SCLK) (mpu off)

Linux version 3.3.0-ADI-2012R1-pre-00789-gf281a9b (test@uclinux63-527-usbdev) (gcc version 4.3.5 (ADI-trunk/svn-5764) ) #243 Thu2

SEQUENCER STATUS:               Not tainted

SEQSTAT: 00002027  IPEND: 0008  IMASK: ffff  SYSCFG: 0006

  EXCAUSE   : 0x27

  physical IVG3 asserted : <0xffa00728> { _trap + 0x0 }

RETE: <0x00000000> /* Maybe null pointer? */

RETN: <0x02bd6000> /* kernel dynamic memory */

RETX: <0x00000480> /* Maybe fixed code section */

RETS: <0x02b80394> [ setrlimit01 + 0x354 ]

PC  : <0x02b8556c> [ setrlimit01 + 0x552c ]

DCPLB_FAULT_ADDR: <0x00000000> /* Maybe null pointer? */

ICPLB_FAULT_ADDR: <0x02b8556c> [ setrlimit01 + 0x552c ]

PROCESSOR STATE:

R0 : 00000000    R1 : 00000061    R2 : 00000005    R3 : 00000000

R4 : 02b80800    R5 : 02b8b91c    R6 : 00000000    R7 : 00000000

P0 : 00000000    P1 : 0000000a    P2 : 00000005    P3 : 02b8d129

P4 : 00000001    P5 : 02b8fe60    FP : 02ba3ef8    SP : 02bd5f24

LB0: 02b8556d    LT0: 02b8556a    LC0: 00000005

LB1: 02b89041    LT1: 02b88ff6    LC1: 00000000

B0 : 00000000    L0 : 00000000    M0 : 00000000    I0 : 02ba2ec8

B1 : 00000000    L1 : 00000000    M1 : 00000000    I1 : 02b8eb8c

B2 : 00000000    L2 : 00000000    M2 : 00000000    I2 : 00000000

B3 : 00000000    L3 : 00000000    M3 : 00000000    I3 : 00000000

A0.w: 00000035   A0.x: 00000000   A1.w: 00000035   A1.x: 00000000

USP : 02ba3ee4  ASTAT: 02000002

Hardware Trace:

   0 Target : <0x000040c0> { _trap_c + 0x0 }

     Source : <0xffa006bc> { _exception_to_level5 + 0xa4 } CALL pcrel

   1 Target : <0xffa00618> { _exception_to_level5 + 0x0 }

     Source : <0xffa004d0> { _bfin_return_from_exception + 0x18 } RTX

   2 Target : <0xffa004b8> { _bfin_return_from_exception + 0x0 }

     Source : <0xffa00572> { _ex_trap_c + 0x72 } JUMP.S

   3 Target : <0xffa00500> { _ex_trap_c + 0x0 }

     Source : <0xffa00782> { _trap + 0x5a } JUMP (P4)

   4 Target : <0xffa00728> { _trap + 0x0 }

      FAULT : <0x02b8556c> [ setrlimit01 + 0x552c ] B[P0++] = R1  (Z)

     Source : <0x02b8556a> [ setrlimit01 + 0x552a ] R1 = B[P3++] (Z)

   5 Target : <0x02b85562> [ setrlimit01 + 0x5522 ]

     Source : <0x02b85532> [ setrlimit01 + 0x54f2 ] IF CC JUMP pcrel

   6 Target : <0x02b85528> [ setrlimit01 + 0x54e8 ]

     Source : <0x02b80390> [ setrlimit01 + 0x350 ] JUMP.L

   7 Target : <0x02b80386> [ setrlimit01 + 0x346 ]

     Source : <0x02b802d8> [ setrlimit01 + 0x298 ] IF CC JUMP pcrel

   8 Target : <0x02b802be> [ setrlimit01 + 0x27e ]

     Source : <0x02b8350e> [ setrlimit01 + 0x34ce ] RTS

   9 Target : <0x02b8350e> [ setrlimit01 + 0x34ce ]

     Source : <0xffa00070> { _ret_from_fork + 0x70 } RTI

  10 Target : <0xffa00006> { _ret_from_fork + 0x6 }

     Source : <0x00026c80> { _schedule_tail + 0x50 } RTS

  11 Target : <0x00026c7a> { _schedule_tail + 0x4a }

     Source : <0x00026c56> { _schedule_tail + 0x26 } IF CC JUMP pcrel

  12 Target : <0x00026c44> { _schedule_tail + 0x14 }

     Source : <0x0002691a> { _finish_task_switch + 0x4e } RTS

  13 Target : <0x0002690c> { _finish_task_switch + 0x40 }

     Source : <0x00026922> { _finish_task_switch + 0x56 } IF !CC JUMP pcrel (BP)

  14 Target : <0x0002691c> { _finish_task_switch + 0x50 }

     Source : <0x00026906> { _finish_task_switch + 0x3a } IF !CC JUMP pcrel (BP)

  15 Target : <0x000268cc> { _finish_task_switch + 0x0 }

     Source : <0x00026c40> { _schedule_tail + 0x10 } JUMP.L

Userspace Stack

Stack info:

SP: [0x02ba3ee4] <0x02ba3ee4> [ setrlimit01 + 0x23ee4 ]

FP: (0x02ba3f14)

Memory from 0x02ba3ee0 to 02ba4000

02ba3ee0: 02b80290 [02b8eb8c] 02b8f714  00000000  00000000  02b8fe20  02ba3f14  02b80840

02ba3f00: 02b8f714  00000000  02ba3f78  00000064  00000000 (02ba3f34)<02b87108> 00000000

02ba3f20: 00000000  02ba3f78  00000000  00000000  00000000 (00000000) 0299478e  02b8b960

02ba3f40: 0000002f  00000ff3  00000000  0297cfee  029f4fd6  0297cff3  00000000  00000000

02ba3f60: 00000000  02b8b91c  02b8b92e  00000000  029ea854  00000001  02ba3f97  00000000

02ba3f80: 02ba3fa3  02ba3fae  02ba3fd1  02ba3fe5  00000000  73000000  6c727465  74696d69

02ba3fa0: 54003130  3d4d5245  756e696c  41500078  2f3d4854  3a6e6962  7273752f  6e69622f

02ba3fc0: 62732f3a  2f3a6e69  2f727375  6e696273  53554800  45565f48  4f495352  2e313d4e

02ba3fe0: 342e3831  44575000  2f002f3d  2f6e6962  72746573  696d696c  00313074  00000000

Return addresses in stack:

   frame  1 : <0x02b87108> [ setrlimit01 + 0x70c8 ]

setrlimit01    2  TPASS  :  RLIMIT_FSIZE test PASSED

setrlimit01    3  TPASS  :  RLIMIT_NPROC functionality is correct

setrlimit01    4  TPASS  :  RLIMIT_CORE functionality is correct

root:/>

--

Follow-ups

--- Bob Liu                                                  2012-08-13 04:26:57

can't repeat

--- Vivi Li                                                  2012-09-20 04:17:56

I can't see this crash now.

Close it.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.