Article [#7335] [ltp] ltp test case mmap10 in ltp-full-20120903 fails

[#7335] [ltp] ltp test case mmap10 in ltp-full-20120903 fails

Submitted By: Vivi Li

Open Date

2012-09-17 06:03:21     Close Date

2012-09-20 03:39:04

Priority:

Medium     Assignee:

Nobody

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

ALL     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Rejected

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.3-2012_Sep_11

App binary format:

N/A     

Summary: [ltp] ltp test case mmap10 in ltp-full-20120903 fails

Details:

ltp test case mmap10 in ltp-full-20120903 fails after apply bellow patch.

--

root:/> mmap10

mmap10      0  TINFO  :  use /dev/zero.

mmap10      0  TINFO  :  start tests.

mmap10      1  TFAIL  :  munmap: errno=EINVAL(22): Invalid argument

mmap10      2  TFAIL  :  subsequent munmap #1: errno=EINVAL(22): Invalid argument

mmap10      3  TFAIL  :  subsequent munmap #2: errno=EINVAL(22): Invalid argument

mmap10      4  TFAIL  :  child exit status is 1

mmap10      5  TFAIL  :  child exit status is 1

mmap10      6  TFAIL  :  child exit status is 1

root:/>

--

Bellow is the patch:

--

Index: testcases/kernel/syscalls/mmap/mmap10.c

===================================================================

--- testcases/kernel/syscalls/mmap/mmap10.c     (revision 220)

+++ testcases/kernel/syscalls/mmap/mmap10.c     (working copy)

@@ -135,42 +135,57 @@

        }

        if (x == MAP_FAILED)

                tst_brkm(TFAIL|TERRNO, cleanup, "mmap");

+

+#ifndef UCLINUX

#ifdef HAVE_MADV_MERGEABLE

        if (opt_ksm) {

                if (madvise(x, SIZE+SIZE-ps, MADV_MERGEABLE) == -1)

                        tst_brkm(TBROK|TERRNO, cleanup, "madvise");

        }

#endif

+#endif

        x[SIZE] = 0;

-       switch(n = fork()) {

+       switch(n = FORK_OR_VFORK()) {

        case -1:

                tst_brkm(TBROK|TERRNO, cleanup, "fork");

        case 0:

                if (munmap(x+SIZE+ps, SIZE-ps-ps) == -1)

                        tst_brkm(TFAIL|TERRNO, cleanup, "munmap");

+#ifdef UCLINUX

+                _exit(0);

+#else

                exit(0);

+#endif

        default:

                break;

        }

-       switch(n = fork()) {

+       switch(n = FORK_OR_VFORK()) {

        case -1:

                tst_brkm(TBROK|TERRNO, cleanup, "fork");

        case 0:

                if (munmap(x+SIZE+ps, SIZE-ps-ps) == -1)

                        tst_brkm(TFAIL|TERRNO, cleanup,

                                        "subsequent munmap #1");

+#ifdef UCLINUX

+                _exit(0);

+#else

                exit(0);

+#endif

        default:

-               switch (n = fork()) {

+               switch (n = FORK_OR_VFORK()) {

                case -1:

                        tst_brkm(TBROK|TERRNO, cleanup, "fork");

                case 0:

                        if (munmap(x+SIZE+ps, SIZE-ps-ps) == -1)

                                tst_brkm(TFAIL|TERRNO, cleanup,

                                                "subsequent munmap #2");

+#ifdef UCLINUX

+                        _exit(0);

+#else

                        exit(0);

+#endif

                default:

                        break;

                }

--

Follow-ups

--- Bob Liu                                                  2012-09-19 02:53:24

nommu doesn't suuport this.

mmap(/dev/zero) return a address, munmap(address+offset) will cause check in

nommu.c fail

1687         if (vma->vm_file) {

1688                 do {

1689                         if (start > vma->vm_start) {

1690                                 kleave(" = -EINVAL [miss]");

1693                                 return -EINVAL;

--- Vivi Li                                                  2012-09-20 04:40:03

OK, disable mmap10 test case and need to push to upstream.

Close it.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.