Post Go back to editing

Can not open stream on bf537

Hello!

I'm trying to start lighttpd on bf537 (distr 2011RC3). I compiled it and uploaded to my development board? but when I trying to run bin file it returns error for me:

root:/mnt/station/lighttpd> sbin/bfin-linux-uclibc-lighttpd -D -f /mnt/station/lighttpd/conf/lighttpd.conf

19m0-01-25 23:45:53: (configfile.c.901) opening configfile  /mnt/station/lighttpd/conf/lighttpd.conf failed: No such device unmap of memory not mmapped by process 199 (bfin-linux-ucli): 0xffffffff-0x1ffe

As printed above the error was occurred in configfile.c file on 901 line. It's a error log of stream_open function:

if (0 != stream_open(&s, filename)) {

                    if (s.size == 0) {

                              /* the file was empty, nothing to parse */

                              ret = 0;

                    } else {

                              log_error_write(srv, __FILE__, __LINE__, "sbss", // line 901

                                                  "opening configfile ", filename, "failed:", strerror(errno));

                              ret = -1;

                    }

}

And strerror says that error is: No such device unmap of memory not mmapped by process 199 (bfin-linux-ucli): 0xffffffff-0x1ffe

But the meaning of such error is not clear. What is it about? And does anybody have any ideas how to workaround it or fix?

Thanks.

Parents
  • further investigations shows that error in code (in line with mmap function):

              if (-1 == (fd = open(fn->ptr, O_RDONLY | O_BINARY))) {

                             return -1;

              }

      f->start = mmap(0, f->size, PROT_READ, MAP_SHARED, fd, 0); // here!

      close(fd);

      if (MAP_FAILED == f->start) {

          return -1;

              }

Reply
  • further investigations shows that error in code (in line with mmap function):

              if (-1 == (fd = open(fn->ptr, O_RDONLY | O_BINARY))) {

                             return -1;

              }

      f->start = mmap(0, f->size, PROT_READ, MAP_SHARED, fd, 0); // here!

      close(fd);

      if (MAP_FAILED == f->start) {

          return -1;

              }

Children
No Data