Hello,
as long as I was working with the kernel 2.6.x everything works fine with my custom board. Especially the spi flash was mounted.
U-Boot 2010.06-svn288 (ADI-2010R1-RC2) (Mar 09 2012 - 10:59:18)
CPU: ADSP bf526-0.2 (Detected Rev: 0.2) (spi flash boot)
Board: FHF Indutel-IP
Support: http://blackfin.uclinux.org/
Clock: VCO: 300 MHz, Core: 300 MHz, System: 100 MHz
RAM: 64 MiB
SF: Detected M25P128 with page size 256, total 16 MiB
In: serial
Out: serial
Err: serial
KGDB: [on serial] ready
Turn Relay Off
Net: bfin_mac
Hit any key to stop autoboot: 0
bfin> run flashboot
SF: Detected M25P128 with page size 256, total 16 MiB
16384 KiB M25P128 at 0:1 is now current device
## Booting kernel from Legacy Image at 03000000 ...
Image Name: Linux Kernel and ext2
Image Type: Blackfin Linux Kernel Image (gzip compressed)
Data Size: 7700367 Bytes = 7.3 MiB
Load Address: 00001000
Entry Point: 00228570
Verifying Checksum ... OK
Uncompressing Kernel Image ... OK
Starting Kernel at = 00228570
Linux version 2.6.35.7-ADI-2011R1-pre-svn343 (hh@FHF-Linix-HH) (gcc version 4.3.5 (ADI) ) #11 Wed Apr 25 10:06:36 CEST 2012
register early platform devices
bootconsole [early_shadow0] enabled
bootconsole [early_BFuart0] enabled
early printk enabled on early_BFuart0
Found mtd parition at 0x00240000, (len=0x1000000), moving to 0x02f00000
Board Memory: 64MB
Kernel Managed Memory: 64MB
Memory map:
fixedcode = 0x00000400-0x00000490
text = 0x00001000-0x00169e08
rodata = 0x00169e08-0x001f1ff4
bss = 0x001f2000-0x002058e0
data = 0x002058e0-0x0021e000
stack = 0x0021c000-0x0021e000
init = 0x0021e000-0x00240000
available = 0x00240000-0x02f00000
rootfs = 0x02f00000-0x03f00000
DMA Zone = 0x03f00000-0x04000000
Hardware Trace Active and Enabled
Boot Mode: 3
Blackfin support (C) 2004-2010 Analog Devices, Inc.
Compiled for ADSP-BF526 Rev 0.2
Blackfin Linux support by http://blackfin.uclinux.org/
Processor Speed: 300 MHz core clock and 100 MHz System Clock
NOMPU: setting up cplb tables
Instruction Cache Enabled for CPU0
External memory: cacheable in instruction cache
Data Cache Enabled for CPU0
External memory: cacheable (write-back) in data cache
Built 1 zonelists in Zone order, mobility grouping off. Total pages: 11938
Kernel command line: root=/dev/mtdblock0 rw clkin_hz=25000000 debug earlyprintk=serial,uart0,57600 console=ttyBF0,57600
PID hash table entries: 256 (order: -2, 1024 bytes)
Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)
Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)
Kernel managed physical pages: 12032
Memory available: 45256k/65536k RAM, (136k init code, 1443k kernel code, 721k data, 1024k dma, 572k reserved)
Hierarchical RCU implementation.
RCU-based detection of stalled CPUs is disabled.
Verbose stalled-CPUs detection is disabled.
NR_IRQS:159
Configuring Blackfin Priority Driven Interrupts
console [ttyBF0] enabled, bootconsole disabled
console [ttyBF0] enabled, bootconsole disabled
Calibrating delay loop... 595.96 BogoMIPS (lpj=1191936)
pid_max: default: 32768 minimum: 301
Security Framework initialized
Mount-cache hash table entries: 512
Blackfin Scratchpad data SRAM: 4 KB
Blackfin L1 Data A SRAM: 16 KB (16 KB free)
Blackfin L1 Data B SRAM: 16 KB (16 KB free)
Blackfin L1 Instruction SRAM: 48 KB (35 KB free)
NET: Registered protocol family 16
Blackfin DMA Controller
fhf_1404_init(): registering device resources
bio: create slab <bio-0> at 0
SCSI subsystem initialized
bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@7
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
input: attiny-keypad as /devices/platform/i2c-bfin-twi.0/i2c-0/0-0034/input/input0
i2c-bfin-twi i2c-bfin-twi.0: Blackfin BF5xx on-chip I2C TWI Contoller, regs_base@ffc01400
Advanced Linux Sound Architecture Driver Version 1.0.23.
Switching to clocksource bfin_cs_cycles
musb_hdrc: version 6.0, musb-dma, host, debug=0
musb_hdrc: ConfigData=0x00 (UTMI-8)
musb_hdrc: kernel must blacklist external hubs
musb_hdrc: HDRC RTL version 1.900
musb_hdrc musb_hdrc.0: MUSB HDRC host driver
musb_hdrc musb_hdrc.0: new USB bus registered, assigned bus number 1
musb_hdrc musb_hdrc.0: supports USB remote wakeup
usb usb1: default language 0x0409
usb usb1: udev 1, busnum 1, minor = 0
usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb1: Product: MUSB HDRC host driver
usb usb1: Manufacturer: Linux 2.6.35.7-ADI-2011R1-pre-svn343 musb-hcd
usb usb1: SerialNumber: musb_hdrc.0
usb usb1: usb_probe_device
usb usb1: configuration #1 chosen from 1 choice
usb usb1: adding 1-0:1.0 (config #1, interface 0)
hub 1-0:1.0: usb_probe_interface
hub 1-0:1.0: usb_probe_interface - got id
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
hub 1-0:1.0: standalone hub
hub 1-0:1.0: individual port power switching
hub 1-0:1.0: no over-current protection
hub 1-0:1.0: power on to power good time: 10ms
hub 1-0:1.0: local power source is good
hub 1-0:1.0: enabling power on all ports
musb_hdrc musb_hdrc.0: USB Host mode controller at ffc03800 using DMA, IRQ 59
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 2048 (order: 2, 16384 bytes)
TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
TCP: Hash tables configured (established 2048 bind 2048)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
Setting up Blackfin MMR debugfs
hub 1-0:1.0: state 7 ports 1 chg 0000 evt 0000
JFFS2 version 2.2. (NAND) (SUMMARY) �
2001-2006 Red Hat, Inc.
msgmni has been set to 88
io scheduler noop registered
io scheduler cfq registered (default)
bfin-jtag-comm: initialized
bfin-dma: initialized
bfin-uart: Blackfin serial driver
bfin-uart.0: ttyBF0 at MMIO 0xffc00400 (irq = 29) is a BFIN-UART
bfin-uart.1: ttyBF1 at MMIO 0xffc02000 (irq = 31) is a BFIN-UART
brd: module loaded
uclinux[mtd]: RAM probe address=0x2f00000 size=0x1000000
Creating 1 MTD partitions on "RAM":
0x000000000000-0x000001000000 : "ROMfs"
m25p80 spi0.1: m25p128 (16384 Kbytes)
Creating 3 MTD partitions on "m25p128":
0x000000000000-0x000000080000 : "bootloader(spi 512 kB)"
0x000000080000-0x000000600000 : "persistent files(spi 5.5 MB)"
0x000000600000-0x000001000000 : "uImage.ext2(spi 10 MB)"
bfin_mii_bus: probed
bfin_mac: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:00, irq=-1, mdc_clk=2500000Hz(mdc_div=19)@sclk=100MHz)
bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
mice: PS/2 mouse device common for all mice
i2c /dev entries driver
bfin-wdt: initialized: timeout=2 sec (nowayout=1)
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
No device for DAI MAX9851
dma rx:5 tx:6, err irq:16, regs:ffc00900
bf5xx_max9851_init 140 enter
bf5xx_max9851_init platform_device_alloc OK
max9851 Audio Codec 0.5
dma_alloc_init: dma_page @ 0x011a3000 - 256 pages at 0x03f00000
asoc: MAX9851 <-> bf5xx-i2s mapping ok
bf5xx_max9851_init add: 0
ALSA device list:
#0: bf5xx_max9851 (MAX9851)
nf_conntrack version 0.5.0 (707 buckets, 2828 max)
ip_tables: (C) 2000-2006 Netfilter Core Team
TCP cubic registered
NET: Registered protocol family 17
VFS: Mounted root (ext2 filesystem) on device 31:0.
Freeing unused kernel memory: 136k freed
set relay off
probing persistent memory
mounted persistent memory
Network setup
eth0 is 192.168.40.111 netmask 255.255.255.0, default route is 192.168.40.1
enviroment setup
Staring Asterisk
Waiting for Asterisk
[Jan 1 00:00:03] NOTICE[282]: cdr.c:1449 do_reload: CDR simple logging enabled.
[Jan 1 00:00:03] NOTICE[282]: loader.c:1006 load_modules: 20 modules will be loaded.
PHY: 0:00 - Link is Up - 100/Full
Starting telefon
_____________________________________
a8888b. / Welcome to the uClinux distribution \
d888888b. / _ _ \
8P"YP"Y88 / | | |_| __ __ (TM) |
8|o||o|88 _____/ | | _ ____ _ _ \ \/ / |
8' .88 \ | | | | _ \| | | | \ / |
8`._.' Y8. \ | |__ | | | | | |_| | / \ |
d/ `8b. \ \____||_|_| |_|\____|/_/\_\ |
dP . Y8b. \ For embedded processors including |
d8:' " `::88b \ the Analog Devices Blackfin /
d8" 'Y88b \___________________________________/
:8P ' :888
8a. : _a88P For further information, check out:
._/"Yaa_: .| 88P| - http://blackfin.uclinux.org/
\ YP" `| 8P `. - http://docs.blackfin.uclinux.org/
/ \.___.d| .' - http://www.uclinux.org/
`--..__)8888P`._.' jgs/a:f - http://www.analog.com/blackfin
Have a lot of fun...
BusyBox v1.16.2 (2012-04-25 09:53:08 CEST) hush - the humble shell
root:/> version
kernel: Linux release 2.6.35.7-ADI-2011R1-pre-svn343, build #11 Wed Apr 25 10:06:36 CEST 2012
toolchain: bfin-linux-uclibc-gcc release gcc version 4.3.5 (ADI)
user-dist: release svn-356, build #260 Wed Apr 25 10:07:05 CEST 2012
But I had to update the kernel. Basically I copied the 3.2.0 Kernel into trunk and implemented a switch, so that I can change between the old and the new kernel via make menuconfig. The new kernel complies without errors and everything seems to be all right, but the spi flash is not mounted anymore.
U-Boot 2010.06-svn288 (ADI-2010R1-RC2) (Mar 09 2012 - 10:59:18)
CPU: ADSP bf526-0.2 (Detected Rev: 0.2) (spi flash boot)
Board: FHF Indutel-IP
Support: http://blackfin.uclinux.org/
Clock: VCO: 300 MHz, Core: 300 MHz, System: 100 MHz
RAM: 64 MiB
SF: Detected M25P128 with page size 256, total 16 MiB
In: serial
Out: serial
Err: serial
KGDB: [on serial] ready
Turn Relay Off
Net: bfin_mac
Hit any key to stop autoboot: 0
Using bfin_mac device
TFTP from server 192.168.40.34; our IP address is 192.168.40.111
Filename 'uImage.ext2'.
Load address: 0x3000000
Loading: #################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#####################################
done
Bytes transferred = 5302650 (50e97a hex)
## Booting kernel from Legacy Image at 03000000 ...
Image Name: Linux Kernel and ext2
Image Type: Blackfin Linux Kernel Image (gzip compressed)
Data Size: 5302586 Bytes = 5.1 MiB
Load Address: 00001000
Entry Point: 001f598c
Verifying Checksum ... OK
Uncompressing Kernel Image ... OK
Starting Kernel at = 001f598c
Linux version 3.0.8-ADI-2011R1 (hh@FHF-Linix-HH) (gcc version 4.3.5 (ADI) ) #3 Fri May 4 10:03:38 CEST 2012
register early platform devices
Found mtd parition at 0x0020c000, (len=0x1000000), moving to 0x02f00000
Board Memory: 64MB
Kernel Managed Memory: 64MB
Memory map:
fixedcode = 0x00000400-0x00000490
text = 0x00001000-0x00156cb8
rodata = 0x00156cb8-0x001cbbe4
bss = 0x001cc000-0x001de0ec
data = 0x001de0ec-0x001f2000
stack = 0x001f0000-0x001f2000
init = 0x001f2000-0x0020c000
available = 0x0020c000-0x02f00000
rootfs = 0x02f00000-0x03f00000
DMA Zone = 0x03f00000-0x04000000
Hardware Trace active and enabled
Boot Mode: 3
Blackfin support (C) 2004-2010 Analog Devices, Inc.
Compiled for ADSP-BF526 Rev 0.2
Blackfin Linux support by http://blackfin.uclinux.org/
Processor Speed: 300 MHz core clock and 75 MHz System Clock
boot memmap: 000000000020c000 - 0000000002f00000 (usable)
On node 0 totalpages: 12032
free_area_init_node: node 0, pgdat 001ef384, node_mem_map 0020e000
DMA zone: 94 pages used for memmap
DMA zone: 0 pages reserved
DMA zone: 11938 pages, LIFO batch:0
NOMPU: setting up cplb tables
Instruction Cache Enabled for CPU0
External memory: cacheable in instruction cache
Data Cache Enabled for CPU0
External memory: cacheable (write-back) in data cache
pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768
pcpu-alloc: [0] 0
Built 1 zonelists in Zone order, mobility grouping off. Total pages: 11938
Kernel command line: root=/dev/mtdblock0 rw clkin_hz=25000000 debug earlyprintk=serial,uart0,57600 console=ttyBF0,57600 ip=192.168.40.111:192.168.40.34:192.f
PID hash table entries: 256 (order: -2, 1024 bytes)
Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)
Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)
Kernel managed physical pages: 12032
Memory available: 45424k/65536k RAM, (104k init code, 1367k kernel code, 621k data, 1024k dma, 612k reserved)
NR_IRQS:159
Configuring Blackfin Priority Driven Interrupts
console [ttyBF0] enabled
Calibrating delay loop... 594.88 BogoMIPS (lpj=990208)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 512
Blackfin Scratchpad data SRAM: 4 KB
Blackfin L1 Data A SRAM: 16 KB (16 KB free)
Blackfin L1 Data B SRAM: 16 KB (16 KB free)
Blackfin L1 Instruction SRAM: 48 KB (36 KB free)
NET: Registered protocol family 16
Blackfin DMA Controller
ezkit_init(): registering device resources
bio: create slab <bio-0> at 0
SCSI subsystem initialized
i2c-bfin-twi i2c-bfin-twi.0: Blackfin BF5xx on-chip I2C TWI Contoller, regs_base@ffc01400
Advanced Linux Sound Architecture Driver Version 1.0.24.
Switching to clocksource bfin_cs_cycles
Switched to NOHz mode on CPU #0
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 2048 (order: 2, 16384 bytes)
TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
TCP: Hash tables configured (established 2048 bind 2048)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
JFFS2 version 2.2. (NAND) (SUMMARY) �
2001-2006 Red Hat, Inc.
msgmni has been set to 88
io scheduler noop registered
io scheduler cfq registered (default)
bfin-uart: Blackfin serial driver
bfin-uart.0: ttyBF0 at MMIO 0xffc00400 (irq = 29) is a BFIN-UART
bfin-uart.1: ttyBF1 at MMIO 0xffc02000 (irq = 31) is a BFIN-UART
bfin-jtag-comm: initialized
bfin-dma: initialized
brd: module loaded
uclinux[mtd]: RAM probe address=0x2f00000 size=0x1000000
Creating 1 MTD partitions on "RAM":
0x000000000000-0x000001000000 : "ROMfs"
bfin_mii_bus: probed
bfin_mac: attached PHY driver [Micrel KS8051] (mii_bus:phy_addr=0:00, irq=-1, mdc_clk=2500000Hz(mdc_div=14)@sclk=75MHz)
bfin_mac bfin_mac.0: eth0: Blackfin on-chip Ethernet MAC driver, Version 1.1
mousedev: PS/2 mouse device common for all mice
i2c /dev entries driver
bfin-wdt: initialized: timeout=20 sec (nowayout=1)
ALSA device list:
No soundcards found.
nf_conntrack version 0.5.0 (709 buckets, 2836 max)
ip_tables: (C) 2000-2006 Netfilter Core Team
TCP cubic registered
NET: Registered protocol family 17
dma_alloc_init: dma_page @ 0x002fb000 - 256 pages at 0x03f00000
IP-Config: Complete:
device=eth0, addr=192.168.40.111, mask=255.255.255.0, gw=192.168.40.2,
host=FHF, domain=, nis-domain=(none),
bootserver=192.168.40.34, rootserver=192.168.40.34, rootpath=
VFS: Mounted root (ext2 filesystem) on device 31:0.
Freeing unused kernel memory: 104k freed
Waiting for Asterisk
PHY: 0:00 - Link is Up - 100/Full
_____________________________________
a8888b. / Welcome to the uClinux distribution \
d888888b. / _ _ \
8P"YP"Y88 / | | |_| __ __ (TM) |
8|o||o|88 _____/ | | _ ____ _ _ \ \/ / |
8' .88 \ | | | | _ \| | | | \ / |
8`._.' Y8. \ | |__ | | | | | |_| | / \ |
d/ `8b. \ \____||_|_| |_|\____|/_/\_\ |
dP . Y8b. \ For embedded processors including |
d8:' " `::88b \ the Analog Devices Blackfin /
d8" 'Y88b \___________________________________/
:8P ' :888
8a. : _a88P For further information, check out:
._/"Yaa_: .| 88P| - http://blackfin.uclinux.org/
\ YP" `| 8P `. - http://docs.blackfin.uclinux.org/
/ \.___.d| .' - http://www.uclinux.org/
`--..__)8888P`._.' jgs/a:f - http://www.analog.com/blackfin
Have a lot of fun...
BusyBox v1.16.2 (2012-05-04 09:11:39 CEST) hush - the humble shell
root:/> version
kernel: Linux release 3.0.8-ADI-2011R1, build #3 Fri May 4 10:03:38 CEST 2012
toolchain: bfin-linux-uclibc-gcc release gcc version 4.3.5 (ADI)
user-dist: release svn-356, build #321 Fri May 4 10:03:22 CEST 2012
Attached are the boardfile and the kernel-config.
What am I doing wrong? Why is the spi-flash not mounted anymore. I also went through the boardfile of the ezkit, in order to check, that the symbols are the same, but that did not help me either. Does anyone has an idea or tip??
Thanks for your time and your help