Dear Blackfin uClinux maintainers,
We're committed to support our ADSP-BF527 powered TLL6527M platform with the Blackfin uClinux distribution. I would like to share update summary on our progress so far.
-> RTC - fine
-> GPIO access - fine
-> Timers - char nodes instantiate fine but show busy while opening the the devices nodes
We'll describe the issue in details in a separate thread
-> ADI accelerometer ADXL345 -fine
-> ADI power monitor ADM1192 -fine
-> ADI temperature sensor ADT75 - fine
-> ADI captouch controller AD7147 - fine
-> ADI Touch screen controller AD7879 - fine
-> ADI GPIO Expander ADP5588 - fine
-> ADI Audio CODEC SSM2602 (tested with ALSA, amixer, arecord, aplay, vrec, vplay, mp3player, ran into issue with mixer posted separately) - fine
-> spi_dev - fine
-> 8GB sdcard over mmc_spi - fine
-> Ethernet : using ftp and telnet console - fine
-> USB host mode: Pendrives, webcam QVGA mode - fine
-> fb using SHARP LQ035Q1 display (same as ADI LCD extender) -fine
Although the video_test runs fine and images get displayed, we see a lot of error messages. We'll describe the issue in details in a separate thread
-> jffs2 : Faced issue compiling mtd-utlis and jffs2, missing header file uuid.h, we've posted this separately, follow up on suggestions and report back
USB Webcam VGA image capture fails: -
Then there is the outstanding issue of capturing images of resolution greater than QVGA using logitech USB webcams, documented here (http://blackfin.uclinux.org/gf/project/u-boot/forum/?_forum_action=ForumMessageBrowse&thread_id=45214&action=ForumBrowse&forum_id=39). This issue has been persisting from 2010R1 and we see the same behaviour on 2011R1. During your 2011R1-RC1 testing and validation, are there any plans to test the USB webcam image capture at resolutions higher than QVGA?
Best regards,
Ashish Gupta
The Learning Labs