bf516 network sometimes become very slow

Hi,

      My  product solution is to use bf516 v0.2 work under uClinux environment. The phy device is smsc 8710. This product has been manufactured three years ago no attention to network issue, recently I discovered a problem with the network.When product work for some time (perhaps a few days or a few hours), the network is very slow. The product network display:

 

      eth0      Link encap:Ethernet  HWaddr 00:05:F7:C0:0A:4C                        
          inet addr:192.168.1.236  Bcast:192.168.1.255  Mask:255.255.255.0     
          UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1                   
          RX packets:59216 errors:0 dropped:0 overruns:0 frame:0               
          TX packets:501 errors:0 dropped:0 overruns:0 carrier:0               
          collisions:0 txqueuelen:1000                                         
          RX bytes:4180523 (3.9 MiB)  TX bytes:53954 (52.6 KiB)                
                                                                               
lo        Link encap:Local Loopback                                            
          inet addr:127.0.0.1  Mask:255.0.0.0                                  
          UP LOOPBACK RUNNING  MTU:16436  Metric:1                             
          RX packets:3 errors:0 dropped:0 overruns:0 frame:0                   
          TX packets:3 errors:0 dropped:0 overruns:0 carrier:0                 
          collisions:0 txqueuelen:0                                            
          RX bytes:336 (336.0 B)  TX bytes:336 (336.0 B)

 

 

    PC  ping the device:

chlxie@ubuntu:~$ ping 192.168.1.236
PING 192.168.1.236 (192.168.1.236) 56(84) bytes of data.
From 192.168.1.214 icmp_seq=1 Destination Host Unreachable
From 192.168.1.214 icmp_seq=2 Destination Host Unreachable
From 192.168.1.214 icmp_seq=3 Destination Host Unreachable
64 bytes from 192.168.1.236: icmp_req=4 ttl=64 time=1001 ms
64 bytes from 192.168.1.236: icmp_req=5 ttl=64 time=1.81 ms
64 bytes from 192.168.1.236: icmp_req=6 ttl=64 time=0.989 ms
64 bytes from 192.168.1.236: icmp_req=7 ttl=64 time=0.813 ms
64 bytes from 192.168.1.236: icmp_req=8 ttl=64 time=0.839 ms
64 bytes from 192.168.1.236: icmp_req=9 ttl=64 time=0.969 ms
64 bytes from 192.168.1.236: icmp_req=10 ttl=64 time=0.765 ms
64 bytes from 192.168.1.236: icmp_req=11 ttl=64 time=0.793 ms
64 bytes from 192.168.1.236: icmp_req=12 ttl=64 time=1.02 ms
64 bytes from 192.168.1.236: icmp_req=21 ttl=64 time=1.02 ms
64 bytes from 192.168.1.236: icmp_req=22 ttl=64 time=0.853 ms
64 bytes from 192.168.1.236: icmp_req=23 ttl=64 time=0.825 ms
64 bytes from 192.168.1.236: icmp_req=24 ttl=64 time=0.851 ms
64 bytes from 192.168.1.236: icmp_req=25 ttl=64 time=0.953 ms
64 bytes from 192.168.1.236: icmp_req=26 ttl=64 time=0.979 ms
64 bytes from 192.168.1.236: icmp_req=27 ttl=64 time=0.835 ms
64 bytes from 192.168.1.236: icmp_req=28 ttl=64 time=0.837 ms
64 bytes from 192.168.1.236: icmp_req=29 ttl=64 time=0.970 ms
64 bytes from 192.168.1.236: icmp_req=4 ttl=64 time=25028 ms (DUP!)
64 bytes from 192.168.1.236: icmp_req=14 ttl=64 time=15021 ms
64 bytes from 192.168.1.236: icmp_req=15 ttl=64 time=14021 ms
64 bytes from 192.168.1.236: icmp_req=16 ttl=64 time=13021 ms
64 bytes from 192.168.1.236: icmp_req=17 ttl=64 time=12021 ms
64 bytes from 192.168.1.236: icmp_req=18 ttl=64 time=11021 ms
64 bytes from 192.168.1.236: icmp_req=19 ttl=64 time=10019 ms
64 bytes from 192.168.1.236: icmp_req=20 ttl=64 time=9012 ms

 

    Network cable is connect normal. I began to suspect that there is a problem by phy 8710, I let 8710 hardware reset, but the network still has the problem. If want the network back to normal, must input "ifconfig eth0 down and ifconfig eth0 up"。 If not doing anything, wait for some hours(specific time can not be determined),the network back to normal.  I try to control the mac register, turn off the emac and turn on the emac  that is not change network to fine.

      linux verion is  2.6.34.7-ADI-2010R1, update to  blackfin-buildroot-2013R1-RC2   is also have the same problem.

     Please help me to solve the problem, thank you very much.