Post Go back to editing

Qt project with mcapi

Hi! I want to include MCAPI library in my Qt project. What should I do to make this?

I copied mcapi 2.0 headers into myproject/mcapi folder and append INCLUDEPATH += $$PWD/mcapi into .pro file. Also I appended DEPENDPATH += $$PWD/mcapi and unix:!macx: LIBS += -L$$PWD/mcapi/ -lmcapi. But I get error

mainwindow.o: In function `MainWindow::on_pushButton_2_clicked()':

../myproject/mainwindow.cpp:(.text+0x134): undefined reference to `mcapi_initialize(unsigned int, unsigned int, attributes_t const*, int const*, mcapi_info_t*, unsigned int*)'

collect2: ld returned 1 exit status

Parents
  • I happen to be working with a QT + mcapi demo project recently too. The will be an extra Linux application that will be invoked by the event like clicking a button on QT, this application will include MCAPI in it, to communicate with another core running bare-metal, and this Linux app is quite the same like our existing mcapi msg test code in Linux.

Reply
  • I happen to be working with a QT + mcapi demo project recently too. The will be an extra Linux application that will be invoked by the event like clicking a button on QT, this application will include MCAPI in it, to communicate with another core running bare-metal, and this Linux app is quite the same like our existing mcapi msg test code in Linux.

Children
No Data