Dear All,
I bought a BF537 EZKit Lite development board. I would like to install uClinux in the flash memory of the board.
Actually, I have programmed the flash driver into the board using VDSP, and U-Boot. How can I put uClinux in the flash memory (I have the uClinux for the BF537 STAMP board, that is pretty good also for BF537 EZKit)? Do I need special cables for JTAG interface, or is there a method to interface using the USB cable given with the kit?
Thank you very much for your availability,
Alessandro