Post Go back to editing

ADSP-BF533 doesn't toggle HWAIT with LDR from gnu tool chain

@

Hi All

I found a bug of the Blackfin boot ROM. The ADSP-BF533 doesn't toggle the HWAIT in the slave mode. Let me inform if this is the known issue. I want to know the detail of this bug. Following is silicon bug, but I reported it here to share the info with the GNU tool chain users.

- ADSP-BF533 rev 0.5 silicon

- bfin-elf-ldr 2014R1-RC2

- Workaround : Add "ignore header" at the top of LDR file.


If you generate the LDR by bfin-elf-ldr for SPI slave mode like :


bfin-elf-ldr -T BF533 -c -g 1 jsp.ldr jsp --bmode spi


the ADSP-BF533 doesn't toggle HWAIT. It doen't depend on the PF pin. ( I checked with PF1 and PF13 ). But the generated LDR is completely healthy. I checked it with EE-240, but could not find any bad point in the LDR file.


To solve it, you just have to add the following dummy data at the beginning of LDR file by hand.


0x00 0x00 0x80 0xff     // loading dummy address

0x04 0x00 0x00 0x00     // length (4)

0x32 0x00               // PF1+RESVECT(BF533)+IGNORE

0xDE 0xAD 0xBE 0xEF     // dummy data


Because this is "ignore" block, the header and data are just ignored by boot ROM, but HWAIT toggle.


This problem is not observed if you generate LDR by VDSP elfloader, because the elfloader always add above dummy block for multi DXE boot while you have only one boot DXE.


This issue is not recorded in the silicon anomaly. But if it is known issue, please let me know where I can see the detail .

Parents Reply Children
No Data