Post Go back to editing

BF592 EZ-KIT Jtag Conection using bfin-gdbproxy

Hello,

    I tried to connect BF592 EZ-KIT Lite using the following Jtag command:

         bfin-gdbproxy bfin -connect="cable IGLOO parallel 0x378"

    I got the folowing error:

        error:    bfin: detecting parts failed.

        Segmentation fault.

 

But the in Jtag folder of gcc toolchain, I have a bf592 folder with 2 files: bf592 and STEPPINGS.

So it should be detected. I also tried to use --board=BF592. But I got another error: unknown board BF592   

Anyone knows how to solve this problem? Thanks!

Parents
  • Hi Jie,

       Thank you for your reply. I will try it when I get time (maybe during CNY). I still have a question based on your solution: I connected this BF592 EZ-Kit before via JTAG using ADI original ADZS-USB-ICE.  The software I use is VisualDSP 5.0. But I did not do anything to the JTAG interface. I can single step cod via that JTAG interface.  How did this happen?

Reply
  • Hi Jie,

       Thank you for your reply. I will try it when I get time (maybe during CNY). I still have a question based on your solution: I connected this BF592 EZ-Kit before via JTAG using ADI original ADZS-USB-ICE.  The software I use is VisualDSP 5.0. But I did not do anything to the JTAG interface. I can single step cod via that JTAG interface.  How did this happen?

Children
No Data