Post Go back to editing

BF592 EZ-KIT Jtag Conection using bfin-gdbproxy

Hello,

    I tried to connect BF592 EZ-KIT Lite using the following Jtag command:

         bfin-gdbproxy bfin -connect="cable IGLOO parallel 0x378"

    I got the folowing error:

        error:    bfin: detecting parts failed.

        Segmentation fault.

 

But the in Jtag folder of gcc toolchain, I have a bf592 folder with 2 files: bf592 and STEPPINGS.

So it should be detected. I also tried to use --board=BF592. But I got another error: unknown board BF592   

Anyone knows how to solve this problem? Thanks!

Parents
  • Hi Jie,

         Yes. That IGLOO parallel cable came with HHCN BF531 board, which I bought few years ago and worked all the time with that board. Now I want to tried that cable with BF592 EZ-Kit board. I happened having an old notebook (more than 10 years old) that has a build-in parallel port.

Reply
  • Hi Jie,

         Yes. That IGLOO parallel cable came with HHCN BF531 board, which I bought few years ago and worked all the time with that board. Now I want to tried that cable with BF592 EZ-Kit board. I happened having an old notebook (more than 10 years old) that has a build-in parallel port.

Children
No Data