Post Go back to editing

Linux device driver support

Thread Summary

The user inquired about open-source Linux device driver support for the LTC2873 to enable it on a platform supporting both RS232/485. The support engineer confirmed that only Arduino code is available for the LTC2873, which can be referenced for implementation.
AI Generated Content

Hi All,

 I am start working on LtC2873. Is this micro controller have open source Linux device driver support ? If available send me the inputs

I want to enable Ltc2873 driver on my platform( that support both  both RS232/485)

Thanks,

RajendraPrasad

Edit Notes

added one more line at bottom
[edited by: raje.embd13@gmail.com at 7:54 AM (GMT 0) on 26 Jul 2019]
Parents Reply Children
No Data