ADSP-BF537 Hardware Revision

I've recently got a new batch of boards in where after programming them, I've noticed a warning in the boot dialogue that the OS was compiled for hardware revision 3, but was running on 2. I've looked at the silicon anomaly list for the BF537 but have a hard time determining from it how likely there is to be an issue with running this hardware/software configuration. The specific OS is uCLinux 2008R1.5.

Is it possible/practical to determine interchangeability based on the silicon anomaly list? Or is this one of those "run it and see" type situations? Is the only real answer to re-compile with either 0.2 or "all" version support?