Article [#5938] toolchain-regtest aborts when previous results are missing

[#5938] toolchain-regtest aborts when previous results are missing

Submitted By: Mingquan Pan

Open Date

2010-03-04 04:09:18     Close Date

2010-03-04 23:17:00

Priority:

Medium     Assignee:

Nobody

Board:

N/A     Silicon Revision:

Resolution:

Fixed     Fixed In Release:

N/A

Processor:

ALL     

Host Operating System:

toolchain rev.:

trunk 4.3 head     kernel rev.:

State:

Closed     Found In Release:

2010R1

Is this bug repeatable?:

N/A     

Summary: toolchain-regtest aborts when previous results are missing

Details:

elf-jtag can't test for dir isn't set issue.

Targets:                    elf-jtag

Components:                 binutils gas ld sim gdb newlib gcc g++ gfortran objc libstdc++ libmudflap libgomp

Host:                       i686-pc-linux-gnu

Build:                      i686-pc-linux-gnu

Found multiple versions of runtest, using the one at /usr/bin/runtest

Found multiple versions of bc, using the one at /usr/bin/bc

Found multiple versions of killall, using the one at /usr/bin/killall

Found multiple versions of pstree, using the one at /usr/bin/pstree

Toolchain source:           /home/test/work/cruise/checkouts/toolchain

Path to logs output dir:    /home/test/work/cruise/temp/regtest_build4.3/logs

Path to tests output dir:   /home/test/work/cruise/temp/regtest_build4.3/tests

Path to elf-jtag output dir: /home/test/work/cruise/temp/regtest_build4.3/tests/elf-jtag

Directory does not exist, or is not an absolute path:

  -- /home/test/work/cruise/checkouts/toolchain/buildscript/test_results/elf-jtag

ls: cannot access /home/test/work/cruise/test_scripts/toolchain/toolchain-build/toolchain-2010_Mar_04_09_12/tests/jtag: No such file or directory

ls: cannot access /home/test/work/cruise/test_scripts/toolchain/toolchain-build/lastrun/tests/jtag: No such file or directory

ls: cannot access /home/test/work/cruise/test_scripts/toolchain/toolchain-build/toolchain-2010_Mar_04_09_12/tests/jtag: No such file or directory

Follow-ups

--- Mike Frysinger                                           2010-03-04 17:53:16

you really should be keeping the good test results up-to-date in the

test_results/ ... then this wouldnt be an issue

at any rate, ive made missing previous results a warning instead of a failure

--- Mingquan Pan                                             2010-03-04 23:16:01

I keep the results but not in that folder. We normally set a good test results

locally as standward and compared with it.

Anyway, it is ok now. So close.

--- Mike Frysinger                                           2010-03-05 07:12:22

you should be committing those good standards so that other people can check

them.  our testing behavior should be easily reproducible by others.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.