Power Integrity for High Performance Measurement Systems

    Increasing data rates driven by AI workloads and the evolution from 5G to emerging 6G standards are placing new demands on electronic test and measurement...
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
      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read the Blog:  Simplified I/O: One Chip, Flexible Voltage Output, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Simplified I/O: One Chip, Flexible Voltage Outpu...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

EngineerZone
EngineerZone
Hardware Tools
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Hardware Tools
  • Processors & DSP
  • Software & Development Tools
  • Hardware Tools
  • Cancel
Hardware Tools
Documents Why does the ICE Test pass but IDDE cannot connect to target?
  • Forums
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • +Documents
  • +4010 Custom Resets: FAQ
  • +ADSP Blackfin dev kits: FAQ
  • +ADSP-BF609 EZ-KIT Lite: FAQ
  • +Board Support Package: FAQ
  • +CCES 1.1.0: FAQ
  • +CrossCore Embedded Studio: FAQ
  • +DSP EZ-KIT: FAQ
  • -ICE Test Utility: FAQ
    • Why does the ICE Test pass but IDDE cannot connect to target?
  • +ICE-1000 and ICE-2000: FAQ
  • +In-Circuit Emulator: FAQ
  • +JTAG TCLK: FAQ
  • +Target Connection Error: FAQ
  • +VisualDSP++: FAQ

Why does the ICE Test pass but IDDE cannot connect to target?

Question:

The ICE Test Utility passes, but when I try to connect to my target in the IDDE the connection fails with a target connection error. What is causing this?

===========================

Answer:

The ICE Test utility only talks to the JTAG port on the processor. It sets the processor to bypass mode and shifts bits through the JTAG bypass register. This utility only verifies that the JTAG connection is working, nothing more. These tests do NOT test the /EMU signal, which is specific to ADI and used by our ICEs as a JTAG emulation status flag from the processor.  They also do NOT test for issues like shorts, problems with the processor's pins, etc.

You should also check the state of the bus request signal on power-up and verify that the processor is not stuck in reset.

If you are using a custom board, it is also recommended to consult the 'JTAG Emulation Technical Reference' - EE-68 for details of the JTAG specification and to ensure your board conforms with this standard.

 

More information on possible causes of a Target Connection Error can be found in the ‘Emulator and EZ-KIT Lite Evaluation System Troubleshooting Guide’ - EE-175.The troubleshooting advice in this EE-Note can be used to resolve most installation, connection, and software issues affecting the use of Analog Devices In-Circuit Emulators (ICEs) and EZ-KIT LiteRegistered evaluation systems.

The ICE Test is available from the Target Configurator by clicking the ‘Test…’ button.

[VisualDSP++]

To invoke the VisualDSP++ Configurator from the Windows Start button choose Programs, Analog Devices, VisualDSP 5.0, and then VisualDSP++ Configurator.

[CrossCore Embedded Studio (CCES)]

The Target Configurator is invoked by selecting Debug Configurations from the Run file menu within CrossCore Embedded Studio.

Alternatively you can right-click a project and choose either Run As > Run Configurations or Debug As > Debug Configurations from the context menu. Once the Run/Debug Configurations dialog box appears click Select Session from the Session tab of the Run/Debug Configurations dialog box. The Session Wizard appears.

Click Configurator from any page of the Session wizard to load the Target Configurator.

 

----------

This FAQ was generated from the following thread: Why does the ICE Test pass but IDDE cannot connect to target?

Tags: ice_test tools emulator
  • Share
  • History
  • More