Q:
The BF548 EZ-KIT Lite schematic is missing the Debug Agent interface. Is this part of the schematic available?
----------
A:
The Debug Agent (USB debugger) interface on the EZ-KIT Lite is proprietary. This is implemented by the FPGA and, on newer EZ-KIT Lites, additional BF535 processor.
What is not shown on the schematics:
The EZ-Kit includes hardware consisting of an FPGA on older EZ-KIT Lites, and a BF535 on newer EZ-KIT Lites, which implements two different main functions. It implements a proprietary USB debugger interface for communication between the board and the host PC as well as also implementing a serial port interface for communication between the DSPs and the on-board converters.
Further details of the FPGA/BF535 interface (software and hardware) of this undisclosed section of the EZ-Kit Lite are proprietary and cannot be made available.
----------
This FAQ was generated from the following thread: Why are certain portions of my EZ-KIT Lite schematics missing or not shown?