Q:
Where can I obtain the schematics for the BF537 STAMP board?
..............................
A:
Unfortunately we do not have schematics specifically for the BF537 STAMP board. The design for the BF537 EZ-Kit and BF537 STAMP board are the same. The differences between the two boards are, the STAMP board does not have the audio circuit and the debug agent.
The schematics for the BF537 EZ-Kit are attached to the BF537 EZ-Kit manual, you can find the latest version of this manual in our Technical Library.
For earlier versions of the schematics please refer to our BF537 legacy manuals, which are also available using the link above.