Power Management Fundamentals II Session 5: Deeper Look into Power Protection

    When is the best time to discover your power circuit needs protection? Let's explore the use of some input protection and control options like ideal diodes...
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
      1. Quote of this month: " When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Too Much Chatter and Not Enough Talk - Learn the Benefits...
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
    Achieving Power Over Data with RS-485 Transceivers

    By Bryson Barney What if a single wire could carry both energy and information seamlessly—without either getting in the way? The future of connectivity...

     

    ​​Functional Safety: A Driver of “Shift Left”​

    By Richard Obrien The key to faster, safer product development is to start smart - not catch up hard. In this blog, we’ll explore how the "Shift Left...

    Latest Blogs

    • The 5 Advantages of Hardware Fault Tolerance
    • The Power Problem Inside Every AI Breakthrough: Part 1 of 3
    • Simplifying Stability with EVAL-KW4503Z: Part 1 of 3
    • Energy Transfer Considerations in Isolated SMPS: Part 2 of 4
    • Automating LTspice .NOISE Measurements with .STEP and .MEAS Directives: Part 2 of 3
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
Hardware Tools
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Hardware Tools
  • Processors & DSP
  • Software & Development Tools
  • Hardware Tools
  • Cancel
Hardware Tools
Documents Why do flash contents appear corrupt/incorrect within Memory Window
  • Forums
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • +Documents
  • +4010 Custom Resets: FAQ
  • +ADSP Blackfin dev kits: FAQ
  • +ADSP-BF609 EZ-KIT Lite: FAQ
  • +Board Support Package: FAQ
  • +CCES 1.1.0: FAQ
  • +CrossCore Embedded Studio: FAQ
  • +DSP EZ-KIT: FAQ
  • +ICE Test Utility: FAQ
  • +ICE-1000 and ICE-2000: FAQ
  • +In-Circuit Emulator: FAQ
  • +JTAG TCLK: FAQ
  • +Target Connection Error: FAQ
  • -VisualDSP++: FAQ
    • Can I use the Stand Alone Debug Agent board with my custom board?
    • How can I test for faulty connections between my ICE and Target Board?
    • How do you connect to an ADSP-218x EZ-KIT in VisualDSP++ 3.5?
    • How do you solve "EZ-ICE Driver (Fatal Firmware Error 174)" error?
    • I have an EZ-KIT Lite, but cannot find any example code in the VisualDSP++ installation. Where are these examples?
    • Reading to/Writing From/Loading to SDRAM on older BF533 EZ-KIT Lite with VisualDSP++ 5.0 behaves incorrectly
    • What is the cause of a "Core fault detected before halt at address" error message?
    • What is the difference between the ADDS and ADZS part numbers?
    • Where can I obtain information regarding the layout and gerber files of my EZ-Kit board
    • Where can I obtain the schematics for the BF537 STAMP board? Audit
    • Why do flash contents appear corrupt/incorrect within Memory Window
    • Why do the ADSP-218x DSPs have their own EZ-ICE emulator?

Why do flash contents appear corrupt/incorrect within Memory Window

 

Q:

When viewing Flash contents using the Memory Window, I see incorrect values, and duplicates of the expected values. How can I use the Memory Window to view the contents of Flash.

-----------------------------------------------

A:

If the flash is not a Parallel type, or is connected to the bus in some non-conventional way, such as SPI, PPI or Link Port Interface, then you cannot use the Memory Window to view the contents of the Flash. All reads/writes to this type of flash should be done using a suitable interface application (such as a Flash Programmer Driver).

If the flash is a parallel type flash connected to the ASYNC bus, you should be able to use the Memory window to view its contents. However, due to timing and other considerations when accessing flash, you may experience incorrect data, or repeated data in the memory window when viewing Parallel Flash locations.

This is caused by the optimized techniques the Emulator uses to access memory when reading from the target, some of which are incompatible with the access requirements of flash. For Blackfin processors, you can avoid these problems by enabling the option "Do Single Byte Memory Access" under 'Settings:Target Options' within the IDDE.

Note: Enabling this option disables many of the Emulator's optimized access, and will cause the load time of your DXE to increase significantly. For this reason, we recommend disabling 'Do single byte memory access' for general operation, and enable it only when you need to examine the contents of the Flash.

Tags: idde visualdsp++ build_env
  • Share
  • History
  • More