Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
    • COTS SoMs & Phased Array Solutions for Rapid RF Subsystem Integration
    • LEO Satcom: Application of RF, Mixed-Signal, & Beamforming ICs
    • 3 Real World Methods to Make Your Power Supply More Intelligent
    • Revolutionizing Flow Cytometry: 20-Bit Precision Signal Chain
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC's Quiz AQQ300 about Divisibility by 6

      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Taming the AI Power Storm: Part 2 of 3 Test your...
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
    Clock Tree Design and Why “PLL Locked” Is Not Enough

    In high-performance RF systems, clocking architecture is a foundational element that directly governs signal integrity, synchronization, and overall system...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Improving Industrial Functional Safety Compliance with High Performance Supervisory CircuitsPart 5: Sequencers Eliminate Systematic Failures

    This article shifts focus from managing the quantitative metrics of functional safety toward mastering the qualitative yet equally critical challenge:...

EngineerZone
EngineerZone
Hardware Tools
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Hardware Tools
  • Processors & DSP
  • Software & Development Tools
  • Hardware Tools
  • Cancel
Hardware Tools
Documents How to set the JTAG TCLK Frequency?
  • Forums
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • +Documents
  • +4010 Custom Resets: FAQ
  • +ADSP Blackfin dev kits: FAQ
  • +ADSP-BF609 EZ-KIT Lite: FAQ
  • +Board Support Package: FAQ
  • +CCES 1.1.0: FAQ
  • +CrossCore Embedded Studio: FAQ
  • +DSP EZ-KIT: FAQ
  • +ICE Test Utility: FAQ
  • +ICE-1000 and ICE-2000: FAQ
  • +In-Circuit Emulator: FAQ
  • -JTAG TCLK: FAQ
    • How to set the JTAG TCLK Frequency?
    • Target Connection Errors after writing to flash
  • +Target Connection Error: FAQ
  • +VisualDSP++: FAQ

How to set the JTAG TCLK Frequency?

Question:

How to set the JTAG TCLK Frequency?

Answer:

JTAG TCLK frequency can be set in CrossCore tool via JTAG Frequency Selection dialog box, it is used to test and set the frequency at which the test clock (TCK) runs in the debug perspective.

To access the JTAG Frequency Selection dialog box, choose Target > Settings > JTAG Frequency Selection, after launching a debug configuration,as documented in the help here: CCES>Help > Contents > CrossCoreRegistered Embedded Studio x.x.x > Integrated Development Environment > Debugging Targets > JTAG Frequency.

The blue arrow icon indicates the frequency at which the test clock is currently running. Note: For the ICE-2000 emulator, the arrow icon is not used.

For more details, please refer the chapter 'JTAG/SWD Frequency' for ICE 2000 in the below link:

http://www.analog.com/media/en/dsp-documentation/evaluation-kit-manuals/ICE_emu_1000_2000_rev_manual.pdf

For more details, please refer the chapter 'JTAG Frequency Selection' for HPUSB ICE in the below link:

http://www.analog.com/media/en/dsp-documentation/emulator-manuals/HPUSBICE_man_rev.3.2.pdf

Meanwhile also please look at 'JTAG Frequency Selection' in EE note in the below link:

http://www.analog.com/media/en/technical-documentation/application-notes/EE356.pdf

This document was generated from the following discussion: Changing the JTAG TCK Frequency