Post Go back to editing

Why are certain portions of my EZ-KIT Lite schematics missing or not shown?

The BF548 EZ-KIT Lite schematic is missing the Debug Agent interface. Is this part of the schematic available?

  • CraigG wrote:

    The BF548 EZ-KIT Lite schematic is missing the Debug Agent interface. Is this part of the schematic available?

    The Debug Agent (USB debugger) interface on the EZ-KIT Lite is proprietary. This is implemented by the FPGA and, on newer EZ-KIT Lites, additional BF535 processor.


    What is not shown on the schematics:
    The EZ-Kit includes hardware consisting of an FPGA on older EZ-KIT Lites, and a BF535 on newer EZ-KIT Lites,  which implements two different main  functions. It implements a proprietary USB debugger interface for communication between the board and the host PC as well as also implementing a serial port interface for communication between the DSPs and the on-board converters.

    Further details of the FPGA/BF535 interface (software and hardware) of this undisclosed section of the EZ-Kit Lite are proprietary and cannot be made available.

    Additionally, board design information for all released products can be found via the "EZ-KIT Lite Design Database" link on the Product Information page for the appropriate EZ-KIT Lite, as well as being available on the FTP site at the following location:

    ftp://ftp.analog.com/pub/tools/Hardware/Reference_Designs/

    Please refer to the Readme.txt for a description of the contents of the ZIP files.

  • This question has been closed by the EZ team and is assumed answered.