Post Go back to editing

how two debug tow processor on the JTAG chain?

Thread Summary

The user encountered JTAG emulation issues with a board containing ADSP21061 and MPC860 processors connected in a single JTAG chain. The suggested configurations for Platform 01 and Platform 10 did not resolve the issue. The final response advised checking the board design against Analog Devices' JTAG Emulation Technical Reference (EE-68) and running the ICE Test utility. If problems persist, the user should contact processor.tools.support@analog.com with the board schematic.
AI Generated Content

hi :

     the customer's board contain two processors , one is our ADSP21061 , the other is MPC860 . the two processor is connected in one JTAG chain .

now they encountered the emulatione issue when connecting to the board .

i advised them to configure the sessin as below:

Platform 01 :   device0 - > ADSP-21061, device1 -> unknow

Platform 10 :   device0 - > unknow, device1 -> ADSP-21061

     it seems these configuration can not work as well ,  so could you give some suggestion about this issue? Thanks .

BR

Dell

Parents Reply Children
No Data