Post Go back to editing

what is the difference between ice-1000 and ice-2000?

I've looked all over the place, but can't seem to find what is the difference between these two products, other than one runs JTAG at 5MHz and the other at 46MHz.  I would think for a price differential of 10x that there would be even more features available on the ice-2000, however, all available materials I have downloaded do not indicate any other difference, except the ice-2000 comes in an enclosure.

Parents Reply Children
No Data