I would like to probe several singles of Processors on following evaluation board.
But there are not pin headers on each board.
ADSP-BF707 EZ-KIT Lite
ADSP-SC589 EZ-KIT Lite
ADSP-SC584 EZ-KIT Lite
Each board has Expansion Interface III (EI3).
Can we connect following board to probe singnals or connect other boards ?
For example,
On the EI3 SDP Breakout Board, there are two 120-pin connectors, J1 and J2.
On the ADSP-BF707 EZ-KIT Lite, there are two 120-pin connectors, P1B and P1C.
Can we connect both two connectors each other ?
( I cannot find the mounting positions of each connectors on the PCB ... )
EI3 SDP Breakout Board ( ADZS-BRKOUT-EX3 )
Probing EI3 Extender Board