Post Go back to editing

ICE-1000 issues in CCES 2.12.01 with own ADSP-21469 board

Thread Summary

The user is experiencing a JTAG communication error when starting a debug session with an ADSP-21469 processor on a custom board using CCES 2.12.1 and an ICE1000 emulator, despite the JTAG scan test passing. The final answer suggests checking the JTAG design against the ADI application note (ee-68.pdf) and verifying the emulator cable and custom board schematics. The user confirms using the shipped emulator cable and is the first to work on this specific board.
AI Generated Content
Category: Hardware
Product Number: ADSP-21469

Hi all:

We are new to SHARC processors and the associated dev tools. We have a self-designed board using an ADSP-21469 which also has a JTAG port. We are using CCES 2.12.1 ( the newer 3.0.2 doesn't support the ADSP-21469, apparently) and, as the JTAG interface, an ICE1000 emulator.

Now, when setting up a debug configuration and assigning a debug session using the ICE1000 I get the following:

  • The ICE1000 passes a JTAG scan test and finds the processor target.

/cfs-file/__key/communityserver-discussions-components-files/420/dg1sbg_5F00_screenshot_5F00_ice1000_5F00_test_5F00_ok_5F00_r.pdf

  • When then starting a debug session I get a JTAG communication error:

/cfs-file/__key/communityserver-discussions-components-files/420/dg1sbg_5F00_screenshot_5F00_ice1000_5F00_jtag_5F00_error_5F00_r.pdf

The ICE1000's LED blink sequence during the debug session start:

Now, after having tried to get to understand the problem, I am now at a loss. Any ideas/ hints/ advice greatly appreciated ... Thanks a lot!

Best, Frank

Parents Reply Children
  • Hi ,

    here are the answers to your points in your last post:

    1. I am using the emulator cable (2-meter USB standard-A to mini-B cable) which is shipped with the emulator package.

    2. I do have another Analog Devises dev board ... somewhere ... Still trying to locate it. I will report back on the results ASAP.

    3. This is the first time I am working on this specific board.

    4. I don't have another emulator available.

    I checked the articles and posts in the threads you pointed to but could not find any advice helping me in my case.

    Could you please look further into this? Thanks!

    Best,

       Frank

  • Hi ,

    Had you verify whether the custom board JTAG designed as per the below linked manual?
    https://www.analog.com/media/en/technical-documentation/application-notes/ee-68.pdf

    Also, please review your custom board schematics once.

    If you are able to locate the ADI evaluation board, it would assist in determining whether the issue is related to the emulator or the custom board. Also please verify if the emulator is detected in the 'Device Manager' under 'CrossCore Tools' and Share screenshots of the Device Manager and emulator properties page.

    Regards,
    Santhakumari.V

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.