Post Go back to editing

21569 SOM Fault Light Suddenly Always On

Thread Summary

The user encountered a SYS_FAULT LED issue on a 21569 SOM, which was caused by a failed 25MHz clock output (CLK0) from the oscillator. The problem was resolved by routing the second 25MHz clock output (CLK1) to the DSP clock input. The user is now able to connect the board in debug mode and the SOM is functioning correctly.
AI Generated Content
Category: Hardware
Product Number: EV-21569-SOM

I have been using a 21569 SOM in standalone mode for a few weeks.

The red LED1 fault LED has suddenly started coming on immediately at power up and I can't get it to go off.

Is there anything I can do with the SOM to stop the fault ? Or is it now unusable ?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.