Hello,
I have the error 0x8004801e - USB Data Count Error opning a session to a Blackfin BF518.
If I run the ICE test it works fine without any error.
If I use the ADZS-HPUSB-ICE with other boards with BF518 it works fine.
Before it stopped working I was debugging a test project based on the "FPGA_memory_test" in order to communicate with our FPGA board.
this is the code I run:
*pEBIU_AMBCTL0 = 0xFFFFFFFF;
ssync();
*pEBIU_AMBCTL1 = 0xFFFFFFFF;
ssync();
*pEBIU_AMGCTL = 0x00F3; //AMBEN[0] and CLKOUT
ssync();
#define FPGA_START 0x20000000 // start address of FPGA (uses /AMS0)
#define FPGA_SIZE 0x00000200 //4096 bits
volatile unsigned int *pDst;
int wrBank0 = 0x1234, rdBank0;
pDst = (unsigned int *)FPGA_START;
*pDst = wrBank0;
msWait(1);
rdBank0 = *pDst;
if (rdBank0 != wrBank0)
bError = 0;
Running it in debug it stopped at "*pDst = wrBank0" and the emulator lost connection.
After that I was not able to connect to the target anymore with the error above.
Is it possible that I damaged something running that code?
How can I restore JTAG communication?
Thank you and best regards
Marco