Hi,
The documentation for the ADSZ-ICE-1000 says it is Windows® 8.1, Window 7 compatible. Is it also compatible with Windows 10?
Thanks,
Hi,
The documentation for the ADSZ-ICE-1000 says it is Windows® 8.1, Window 7 compatible. Is it also compatible with Windows 10?
Thanks,
Hi,
Please note that from CCES 2.3.0 on-wards windows 10 operating system is supported. If you are using the CCES supported version for the windows10, then the ADSP-ICE-1000/2000 can be used with windows 10.
If you are using ICE-1000/2000 with the VisualDSP++ in the windows 10 operating system please note that unfortunately we do not support any version of VisualDSP++ on windows 10. It is supported on the following operating systems:
Windows XP Professional SP3 (32-bit only)
Windows Vista Business, Enterprise, or Ultimate SP2 (32-bit only)
Windows 7 Professional, Enterprise, or Ultimate (32 and 64-bit)
Windows 8 Pro or Enterprise (32 and 64-bit)
Also please note that there are no plans to upgrade VDSP++ for windows 10.
While we have had some customers report success using VisualDSP++ with the Windows "Compatibility Mode", this is not something we have tested nor that we support. We can only support customers using the aforementioned supported operating systems for VisualDSP++.
Regards,
Nishanthi.V