Article What examples are included in the Board Support Packages and CrossCore®︎ Embedded Studio?

Question:

I have recently installed CrossCoreRegistered Embedded Studio. Where can I find examples within the installation?

 

==========================

Answer:

The Board Support Package for your evaluation hardware is available to download from the relevant product page. This package provides all the necessary components needed to use your EZ-Board or EZ-Extender with the CrossCoreRegistered Embedded Studio software development tools.

 

There are two categories of HW controllers: On-chip and off-chip. On-chip controllers are defined as controllers that exist in the processor silicon package. Off-chip controllers are defined as controllers that do not exist in the processor silicon package but have been added to the EZ-Board or EZ-Extender.

 

Once you have installed a Board Support Package, it will allow you to connect to your new target board and access additional examples and SSL 2.0 drivers for off-chip controllers, and documentation for the EZ-Board or EZ-Extender.

 

By default, the location of any Board Support Packages you install can be found at “C:\Analog Devices\”, with examples located in a “.\<Your EZ-Board Software Version>\<Your EZ-Board Name>\Examples” directory.

 

All on-chip controller drivers are delivered as part of the CrossCoreRegistered Embedded Studio distribution. You can find example projects in the following directory:

<Install Dir>\CrossCore Embedded Studio x.x.x\Blackfin\Examples

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.