Building errors for ADuCM4x50 on KEIL with FreeRTOSv10.1.1

Get the FreeRTOS 1.3.0 release kit from https://www.analog.com/en/design-center/processors-and-dsp/evaluation-and-development-software/freertos.html#relatedsoftware 
Build the project "Demo\CORTEX_M4_ADuCM4x50_KEIL" and get these errors as:

C:\Keil_v5\ARM\PACK\AnalogDevices\ADuCM4x50_DFP\3.1.0\Source\drivers\uart\adi_uart.c(1075): error:  #167: argument of type "StaticQueue_t *" is incompatible with parameter of type "QueueHandle_t"
EM_PEND(pChannel,ADI_UART_FAILED);
C:\Keil_v5\ARM\PACK\AnalogDevices\ADuCM4x50_DFP\3.1.0\Source\drivers\uart\adi_uart.c(1411): error:  #167: argument of type "StaticQueue_t *" is incompatible with parameter of type "QueueHandle_t"
EM_PEND(pChannel,ADI_UART_FAILED);
C:\Keil_v5\ARM\PACK\AnalogDevices\ADuCM4x50_DFP\3.1.0\Source\drivers\uart\adi_uart.c: 0 warnings, 2 errors

It is ok to work with FreeRTOS 10.0.0.

Steps:

  1. Get the FreeRTOS from https://www.freertos.org/a00104.html 
  2. Get released ADI FreeRTOS 1.3.0 and unzip it into FreeRTOS product
  3. Open this project in "FreeRTOSv10.1.1\FreeRTOS\Demo\CORTEX_M4_ADuCM4x50_KEIL" and build it
  4. And get two errors