Post Go back to editing

CCES Launch issue

Thread Summary

The user is experiencing issues with CCES (version 2.12.1.0) closing with exit code 1 during automated builds using Python. The recommended solution is to use the headless builder (ccesc.exe) and CCES Runner (CCES_runner.exe) for automation, as detailed in the provided Analog Devices FAQs. The user is building a project based on ADSP SC 589, with each core built separately, and the issue occurs randomly during multiple iterations.
AI Generated Content
Category: Software
Product Number: SC 594
Software Version: 3.0.2

Hi,

We are automating the build process using Python wherein the cces is opened, binaries are generated and cces is closed. This process will be iterated say some 10 times in generating necessary binaries from the project. The software version of cces is 2.12.1.0

The problem here is, in some iterations say 5th or 8th, while launching cces, it is closing with exit code1 and cces is abruptly closing. Picture of the same is attached. 

Please help us with this.

Edit Notes

The software version of cces is 2.12.1.0
[edited by: BVS at 11:44 AM (GMT -5) on 20 Feb 2025]

Thread Notes

Parents Reply Children
No Data