Post Go back to editing

Ethernet Usage in BF-609

Category: Software
Product Number: ADSP BF-609
Software Version: Cross Core Embedded Studio 2.11.0.0

HI,

Can you please confirm, am I able to use Ethernet in BF-609, to send and receive data with this version Cross Core Embedded Studio 2.11.0.0
If your answer was Yes then confirm me which drivers I have to add in the project. Or if your answer was No then tell the process(solution) how to clear it in Cross Core Embedded Studio 2.11.0.0.

and Finally suggest me which version(Cross Core Embedded Studio) is good for me to install, regarding Ethernet .

Thanks,

Shiva

  • Hi Shiva,

    Thank you for your inquiry.

    Please find the details for your queries here.

    Can you please confirm, am I able to use Ethernet in BF-609, to send and receive data with this version Cross Core Embedded Studio 2.11.0.0
    >>> Can you please try to run the attached POST code in CCES2.12.0. Few issues in CCES2.11.0 got fixed in this version.

    This issue has been discussed in the below Ezone thread
    Ethernet loopback 

    You can get CCES 2.12.0 from the below link.
    download.analog.com/.../ADI_CrossCoreEmbeddedStudio-Rel2.12.0.exe

    You can refer driver source code from the below CCES Installation path
    C:\Analog Devices\CrossCore Embedded Studio 2.12.0\Blackfin\lib\src\drivers\source\ethernet

    You can get the detailed description of individual APIs from the below help path
    CrossCore® Embedded Studio 2.12.0 > System Run-Time Documentation > System Services and Device Drivers > ADSP-BF60x API Reference > Modules

    Hope this helps.

    Best Regards,
    Santhakumari.V

    Post-Ethernet.zip