Post Go back to editing

ADSP-21489 EZ-Kit Lite connect to PC

Category: Software
Product Number: ADSP-21489
Software Version: VisualDSP++ 5.1.2

Hello everyone,


I use the IDE VisualDSP++ 5.1.2. I have an ADSP-21489 EZ-Kit Lite with revision 1.8 and a SADA2 with revision 1.5. On the SADA2, pins 1 and 2 are connected at JP1.

When running the ICE test, the status "Determining scan path length" gives the error "No JTAG devices detected in the scan path. Check target power and verify JTAG signal integrity".

When I click on Connect from the IDE and the Session Wizard opens, I first select the processor "ADSP-21489". Roof the connection type "EZ-KIT Lite" which results in a platform ADSP-21489 EZ-Kit Lite via Debug Agent. If this is confirmed by Finish, error 0x80048049 appears. What do I have to change so that it works and I can connect the PC to the processor.

In the device manager the board is displayed as "ADI Development Tools" --> "ADSP-21489 EZ-KIT Lite".

Best regards
Tobias