.c files for demo application.

I'm working on ADSP SC589 ez kit and my .c files for arm, SHarc0 and sharc1 for demo application are lost. How can i get them back?

Thanks.

  • Hi,

    Please note that, Typically a project will use a number of relative paths in its configuration that may become invalid once the project has been moved. These are files that do not exist within the directory structure of the project, and are instead linked into the project from relative paths

    To use the linked resources path, please follow the below steps.

    1. Open project properties > Resources > Linked Resources
    2. Select the "Linked Resources" tab which is next to Path Variables.
    3. Select the to be changed to relative location under 'Resource name' and click 'Edit'.
    4. Select the source file/folder to be link and click OK.

    If you need to create a new path variable for any other locations, we recommend to refer the below CCES help page.
    CrossCore® Embedded Studio 2.6.0 > Integrated Development Environment > Managing CCES Projects > Workspace Organization >
    Path Variables

    We recommend to refer the below FAQ which might be helpful:
    FAQ: What changes are needed to build a CrossCore Embedded Studio project after moving to another directory?
    ez.analog.com/.../faq-what-changes-are-needed-to-build-a-crosscore-embedded-studio-project-after-moving-to-another-directory

    If you are still facing issue,please try perform a "Clean Project", available from right clicking on the project in the IDE and rebuild the project,open CCES with the new workspace and import the example and then try to build.

    Regards,
    Santha kumari.K