Displaying a subset of the Linux Add-In's Buildroot variables

With the Linux Add-In v1.2.0 for CCES, why is it that when I follow the Buildroot User Manual section 8.1. "make tips" to display its variables, I seem to get all the (21 MB of) variables, not just the BUSYBOX_%DEPENDENCIES ones, as the example shows.

It is possible to tweak the output using some variables:

 - VARS will limit the listing to variables which names match the specified make-pattern
  ...
 
For example:
 $ make -s printvars VARS=BUSYBOX_%DEPENDENCIES
 BUSYBOX_DEPENDENCIES=skeleton toolchain
 BUSYBOX_FINAL_ALL_DEPENDENCIES=skeleton toolchain
 BUSYBOX_FINAL_DEPENDENCIES=skeleton toolchain
 BUSYBOX_FINAL_PATCH_DEPENDENCIES=
 BUSYBOX_RDEPENDENCIES=ncurses util-linux

I copy-&-paste 'make -s printvars VARS=BUSYBOX_%DEPENDENCIES' directly from the Buildroot User Manual page into my development host's terminal. Is this a problem with the version of Buildroot that's included in the Linux Add-In for CCES v.1.2.0, or is it a problem with the Linux Add-In for CCES v.1.2.0, itself?


Correct URL to 'make tips' page in Buildroot User Manual.
[edited by: jb@hme at 10:25 PM (GMT -4) on 17 Sep 2018]
Parents Reply Children