Open RAN 5G Radio Design: SDR SoCs for Energy-Efficient, Secure Deployments

    Building Secure and Energy‑Efficient 5G Networks with Software Defined Radios. The rapid evolution of 5G networks is driving new requirements for performance...
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
    • Power Integrity for High Performance Measurement Systems
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC Quizzes AQQ302 about Bang Gap Reference Generation

      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

EngineerZone
EngineerZone
CrossCore Embedded Studio and Add-ins
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
CrossCore Embedded Studio and Add-ins
  • Processors & DSP
  • Software & Development Tools
  • CrossCore Embedded Studio and Add-ins
  • Cancel
CrossCore Embedded Studio and Add-ins
Documents Importing and creating multi-core projects in CrossCore Embedded Studio
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • FAQ
  • +a.b silicon into a x.y silicon target: FAQ
  • +accel_xxxx: FAQ
  • +ADC & DAC in audio application: FAQ
  • Add submodule files in CCES
  • +Add version of application in loader file: FAQ
  • Add-in license: FAQ
  • +ADI_SPI_TRANSCEIVER: FAQ
  • +adi_spu_Init() API: FAQ
  • +ADSO-BF609 EZkit: FAQ
  • +ADSP-21364: FAQ
  • +ADSP-214xx: FAQ
  • +ADSP-21569 Ez-kit: FAQ
  • +ADSP-21569: FAQ
  • +ADSP-2183x:FAQ
  • +ADSP-BF609 EZKIT: FAQ
  • +ADSP-BF609: FAQ
  • +ADSP-BF707: FAQ
  • +ADSP-BF70x: FAQ
  • +ADSP-SC589: FAQ
  • +ADSP-SC58x: FAQ
  • +ADSP-SC59x: FAQs
  • +ADSP-SC5xx: FAQ
  • +ADSP-SC8xx FAQs
  • +ADSP21489: FAQ
  • +ADSP215xx: FAQ
  • +alignment pragma: FAQ
  • +ARM CORE: FAQ
  • +ARM to Sharc: FAQ
  • +avoid when a project is getting build: FAQ
  • +BF-609 Evaluation board: FAQ
  • +BF518 Processor: FAQ
  • +BF703: FAQ
  • +BF706 EZ-KIT: FAQ
  • +BF706: FAQ
  • +BF706mini BSP project: FAQ
  • +BF707 SPI: FAQ
  • BITEXP and BITRET for ADSP-214xx
  • C and C++ standard library in CCES?
  • +C source file: FAQ
  • +C++ code: FAQ
  • +C-code ISRs: FAQ
  • cache invalidation and cache flushing
  • +Callback function: FAQ
  • +Calling Library Functions: FAQ
  • +cc1138: FAQ
  • +CCES: FAQ's
  • +cldp: FAQ
  • Clip double precision floating-point in C Audit
  • +CLKIN: FAQ
  • +Code folding in CCES: FAQ
  • +Configuring the Loader, Linker and Archiver: FAQ
  • +connect to the Blackfin: FAQ
  • Create Library files for individual modules Audit
  • Creating and Linking a .dlb in CCES
  • -CrossCore Embedded Studio STDIO: FAQ
    • "DO_CYCLE_COUNTS" macro in CCES
    • Build Configuration settings in CCES
    • Cache settings on SHARC-FX
    • CCES Debug configuration settings
    • CCES_HOME Environment variable
    • Change output directory path of DXE. Audit
    • Compare EV-SOMCRR-EZKIT and EV-SOMCRR-EZLITE
    • Create ASM project in CCES
    • CrossCore Embedded Studio STDIO is slow, and interrupts processing of real world data Audit
    • Default qualifier for the output sections
    • Does CrossCore Embedded Studio have a floating license option?
    • Does CrossCore Embedded Studio Support C++ 11?
    • Dump specific memory contents to a file in CCES
    • Encountering the following error - ‘Invalid license file. The license file may be obsolete, corrupted, missing, or read-only’
    • End of availability for Micrium Add-Ins for CrossCore Embedded Studio
    • Error "Cannot Satisfy Dependency" when installing 3rd Party Plugin under CrossCore Embedded Studio
    • External Configuration tool in CCES
    • FIR Decimation filter
    • FIR interpolation
    • Git-Based Version Control System in CCES
    • How can I issue multiple Pre-Build or Post-Build Commands in CrossCore Embedded Studio
    • How can I obtain the CrossCore Embedded Studio Software License Agreement?
    • How can I obtain university license for Crosscore embedded studio?
    • How do I update the Add-In version being used by my CrossCore Embedded Studio project?
    • How to use custom platform with CCES_Runner.exe Utility
    • ICE feature comparison Table
    • Importing and creating multi-core projects in CrossCore Embedded Studio
    • Instrumented Profiling Report in CCES
    • Is it possible to install both a node-locked license and a corporate domain license on the same machine?
    • Is there any restriction for defining normal-word variables in seg_dmda_nw section on SHARC+?
    • Linking driver source into project
    • MPEG-4 AAC Decoders support on the ADSP-SC573
    • Re-create system.svc
    • Reprogram On-Board Debug Agent Firmware
    • Start/Stop FLEXnet License Server via Command Line
    • Support for Parallel Builds in CrossCore Embedded Studio Audit
    • System Services and Device Drivers for CrossCore®︎ Embedded Studio Training Videos Audit
    • Using Blackfin and SHARC from the command line in CrossCore Embedded Studio
    • Using CMSIS packs from the command line in CrossCore Embedded Studio
    • What are the different types of licenses for CrossCore Embedded Studio? Audit
    • What changes are needed to build a CrossCore Embedded Studio project after moving to another directory? Audit
    • What is the current working directory for the Elfloader in CrossCore Embedded Studio Audit
    • Where can I find details of CrossCore Software and Tools Anomaly Reports? Audit
    • Which versions of CrossCore Embedded Studio (CCES) do I need to install? Audit
  • +CROSSCORE: FAQ
  • Custom debug configurations in CCES
  • +Data Member Alignment: FAQ
  • +Device Driver programming: FAQ
  • Difference between ADZS-HPUSB and ADZS-USB ICE Audit Audit
  • Difference between Debug and Release configurations
  • +Difference between Emulator and Simulator: FAQ
  • +disable prelinker: FAQ
  • DND mode in CCES
  • Does CCES have any API that can be used to build automation test platform with Python Audit
  • Does ICE-1000 supported ADSP-CM407F? Audit
  • +Driver example for Timer windowed watchdog period mode.
  • +Embedded applications: FAQ
  • +EV-21569-SOM: FAQ
  • Example code for SPORT slave trigger in ADSP-21569 Ezkit Audit Audit
  • Export console output to the desired file Audit
  • export/import CCES preferences settings
  • +EXTCLK_MODE: FAQ
  • Flash Programmer Drivers for ADSP-2183x/SC83x and ADSP-SC5xx ARM Cortex A5 Cores
  • GUL-XP board with EZkit license Audit
  • +How to access darkmode appearance in CCES?
  • +How to access stereo channels individually in the Audio_Passthrough_I2S example present in GUL BSP?
  • +How to avoid CORE0 and DEBUG: FAQ
  • How to build a specific code from single source file for a specific core?
  • +How to convert long double into string: FAQ
  • How to create library files for individual modules? Audit
  • +how to deassert Slave: FAQ
  • +How to do profiling: FAQ
  • How to obtain PCB library files for ADI processors Audit
  • How to pass arguments from command line in CCES runner
  • +How to protect shared code/ data: FAQ
  • How To remove automatically added "includes" folders in CCES project Audit
  • How to use "log10f_simd" Audit
  • How to use commands in CCES runner Audit
  • How to use Device programmer in EVAL-ADICUP360 board Audit
  • How to use optimized libraries for FFT Audit
  • +HW Accelerator and SW libraries: FAQ
  • INPUT SECTIONS & INPUT SECTIONS PIN EXCLUSIVE Audit
  • Interrupt header files along with -char-size-32 switch in Sharc Audit
  • +Interrupt Vector Table: FAQ
  • Is it possible to perform stepping into the code in CCES Runner. Audit
  • Is there a way to list symbols from library (*.dlb) file? Audit
  • Is there a way to mangle or remove internal symbols ? Audit
  • JTAG switch Interface for EV-SOMCRR-EZLITE and EV-SOMCRR-EZKIT: Audit
  • +LDF from C code: FAQ
  • +linker map file: FAQ
  • +List of Processors: FAQ
  • +Loader File: FAQ
  • +MCAPI package: FAQ
  • +node-locked license: FAQ
  • +non-blocking peek functions: FAQ
  • Optimization in ARM Audit
  • +PART_SPECIFIC_HEADERS: FAQ
  • +path variables: FAQ
  • +peripheral Error: FAQ
  • +PINT modules: FAQ
  • +PM bus: FAQ
  • +Project Explorer tree: FAQ
  • +PWM mode: FAQ
  • +quad SPI mode: FAQ
  • Reset SHARC core from ARM core using RCU in SC573 Audit
  • +RTOS for older Blackfin or older SHARC: FAQ
  • +SC-573 EZkit: FAQ
  • +SC83x-FAQ
  • +SDRAM: FAQ
  • +SHARC 21469: FAQ
  • +SHARC0: FAQ
  • +SHARC: FAQ
  • +sharing global data between cores: FAQ
  • +SigmaStudioForSHARC: FAQ
  • +SIMD code: FAQ
  • +SIMD: FAQ
  • sizeof() built-in function in BF and Sharc processors Audit
  • +SPI core mode with callback: FAQ
  • +SPI flash: FAQ
  • +SPORT API: FAQ
  • +SPORT: FAQ
  • +SRCU bit: FAQ
  • SRU and DAI routing via GUI
  • +SSLDD 2.0 and SSLDD 3.0: FAQ
  • +SSLDD 3.0: FAQ
  • +SSLDD3.0: FAQ
  • +stack overflow: FAQ
  • +Static library & IP protection: FAQ
  • Streaming Data input and output in CCES
  • +suppress assembler preprocessor warning: FAQ
  • SWD with ICE-1000
  • +system.svc: FAQ
  • TDM with both SPORT channels Audit
  • TWI Transfer using 3.0 APIs
  • +two PINT modules: FAQ
  • +TX and RX DMA Interrupts: FAQ
  • Types of Pragma usage Audit
  • +U-Law and A-Law: FAQ
  • +UART Device Driver: FAQ
  • +UART ISR Callback: FAQ
  • UART sample driver code for BF706mini Audit
  • +VisualDSP++: FAQ
  • +Wakeup processor from Hibernate: FAQ
  • +When callback occurs: FAQ
  • +word addressable program: FAQ
  • [FAQ] : FORCE CONTIGUITY Audit
  • “Peripherals view” in CCES

Importing and creating multi-core projects in CrossCore Embedded Studio

Question

I have a five-project multi-core VisualDSP++ application for ADSP-BF561. How do I use this in CrossCore Embedded Studio?

Answer

You can use the Project Import Wizard to import your project into CrossCore Embedded Studio, and rebuild it there. During the Project Import Wizard, browse to the application's .dpg file. See FAQ: Importing VisualDSP++ project files to CrossCore Embedded Studio for details.

======================================

Question

I want to move my five-project application from ADSP-BF561 to ADSP-BF609. How do I do that?

Answer

The five-project model is not a recommended approach for building multi-core applications for ADSP-BF609, and is not directly supported by CrossCore Embedded Studio. Instead, the recommended approach for ADSP-BF609 applications is to create two separate projects, one per core, which communicate via MCAPI.

 

======================================

Question

Where is libmc for ADSP-BF609?

 

Answer

Libmc is not supported for ADSP-BF609. Instead, the recommended approach for inter-core communication in CrossCore Embedded Studio is MCAPI, an industry-standard approach defined by the Multicore Association.

 

The MCAPI documentation can be found in the CrossCore Embedded Studio Help via 'Help > Contents > CrossCore Embedded Studio 1.0.1 > System Run-Time Documentation > Multicore Communications API (MCAPI) Specification'.

 

======================================

Question

I want to create a new five-project application for ADSP-BF609. Where is that option in the New Project Wizard?

Answer

The New Project Wizard does not support creating new five-project applications. Instead, it creates a two-project application, where each project is a standalone application for its respective core, and MCAPI is used as the communication framework.

 

======================================

Question

I liked the five-project model. Can I still create it myself?

Answer

Yes, although we do not recommend this approach. You can create your own hierarchy of projects (in fact, Eclipse's directory-based project structure encourages this), and this can be a valuable approach for structuring your source code. The linker still supports the COMMON_MEMORY and SHARED_MEMORY constructs that were the basis of the five-project linking approach. However, you will have to manually create the LDFs to use such constructs. Be aware that this is not a trivial task.

 

======================================

Question

How do I go about creating multi-core projects for ADSP-BF561 and ADSP-BF609 in CrossCore Embedded Studio?

Answer

The New Project Wizard creates two projects by default when the processor is BF561 or BF60x. The first project is for core 0/A and the second project is for core 1/B. There is no option in the wizard for “Single Core: Single Application”, “Dual Core: Single Application”, “Dual Core: Single Application using both cores” that were offered in VisualDSP++.

 

======================================

Question

Why have you changed the approach to multicore projects?

Answer

We no longer recommend using the five-project model for starting new projects. The reason for this is that the model was based on using the linker's SHARED_MEMORY and COMMON_MEMORY constructs to create a single application that covered the entire set of memory spaces of both cores. The reason for doing this is so that the linker could arrange for both cores to share code and data, as all symbols were visible across both cores. However, this came with two significant disadvantages. The first is that this approach was incompatible with software not designed for such an architecture - this includes RTOSes and all third-party software. The second is that the memory hierarchy is complex, and it can be difficult to ensure code or data placement to achieve the application's needs - whether they be high-performance, shared, or widely-available. Small changes in application sources could lead to perturbations that were time-consuming to identify, track down and address.

 

In contrast to this, the recommended CrossCore Embedded Studio approach is the two-project approach, also supported in VisualDSP++, although CrossCore Embedded Studio adds the industry-standard MCAPI model for inter-core communication. Because this model keeps each core's applications separate for both code and data, it is much easier to reason about code and data placement, leading to a faster identification of bugs, and a shorter development period.

  • Share
  • History
  • More