Accelerate RF Subsystem Integration with COTS SoMs and Phased Array Solutions. As building a subsystem from early prototype to full deployment is never...
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
      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Taming the AI Power Storm: Part 2 of 3 Test your...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Calibration Implementation Techniques for Multichannel Phased Array Subsystems

    Learn about phase-calibration techniques used for characterizing a 16 transmit and 16 receive X-band phased array subsystem based on a mixed-signal front...

EngineerZone
EngineerZone
CrossCore Embedded Studio and Add-ins
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
CrossCore Embedded Studio and Add-ins
  • Processors & DSP
  • Software & Development Tools
  • CrossCore Embedded Studio and Add-ins
  • Cancel
CrossCore Embedded Studio and Add-ins
Documents Using CMSIS packs from the command line in CrossCore Embedded Studio
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • FAQ
  • +a.b silicon into a x.y silicon target: FAQ
  • +accel_xxxx: FAQ
  • +ADC & DAC in audio application: FAQ
  • Add submodule files in CCES
  • +Add version of application in loader file: FAQ
  • Add-in license: FAQ
  • +ADI_SPI_TRANSCEIVER: FAQ
  • +adi_spu_Init() API: FAQ
  • +ADSO-BF609 EZkit: FAQ
  • +ADSP-21364: FAQ
  • +ADSP-214xx: FAQ
  • +ADSP-21569 Ez-kit: FAQ
  • +ADSP-21569: FAQ
  • +ADSP-2183x:FAQ
  • +ADSP-BF609 EZKIT: FAQ
  • +ADSP-BF609: FAQ
  • +ADSP-BF707: FAQ
  • +ADSP-BF70x: FAQ
  • +ADSP-SC589: FAQ
  • +ADSP-SC58x: FAQ
  • +ADSP-SC59x: FAQs
  • +ADSP-SC5xx: FAQ
  • +ADSP-SC8xx FAQs
  • +ADSP21489: FAQ
  • +ADSP215xx: FAQ
  • +alignment pragma: FAQ
  • +ARM CORE: FAQ
  • +ARM to Sharc: FAQ
  • +avoid when a project is getting build: FAQ
  • +BF-609 Evaluation board: FAQ
  • +BF518 Processor: FAQ
  • +BF703: FAQ
  • +BF706 EZ-KIT: FAQ
  • +BF706: FAQ
  • +BF706mini BSP project: FAQ
  • +BF707 SPI: FAQ
  • BITEXP and BITRET for ADSP-214xx
  • C and C++ standard library in CCES?
  • +C source file: FAQ
  • +C++ code: FAQ
  • +C-code ISRs: FAQ
  • cache invalidation and cache flushing
  • +Callback function: FAQ
  • +Calling Library Functions: FAQ
  • +cc1138: FAQ
  • +CCES: FAQ's
  • +cldp: FAQ
  • Clip double precision floating-point in C Audit
  • +CLKIN: FAQ
  • +Code folding in CCES: FAQ
  • +Configuring the Loader, Linker and Archiver: FAQ
  • +connect to the Blackfin: FAQ
  • Create Library files for individual modules Audit
  • Creating and Linking a .dlb in CCES
  • -CrossCore Embedded Studio STDIO: FAQ
    • "DO_CYCLE_COUNTS" macro in CCES
    • Build Configuration settings in CCES
    • Cache settings on SHARC-FX
    • CCES Debug configuration settings
    • CCES_HOME Environment variable
    • Change output directory path of DXE. Audit
    • Compare EV-SOMCRR-EZKIT and EV-SOMCRR-EZLITE
    • Create ASM project in CCES
    • CrossCore Embedded Studio STDIO is slow, and interrupts processing of real world data Audit
    • Default qualifier for the output sections
    • Does CrossCore Embedded Studio have a floating license option?
    • Does CrossCore Embedded Studio Support C++ 11?
    • Dump specific memory contents to a file in CCES
    • Encountering the following error - ‘Invalid license file. The license file may be obsolete, corrupted, missing, or read-only’
    • End of availability for Micrium Add-Ins for CrossCore Embedded Studio
    • Error "Cannot Satisfy Dependency" when installing 3rd Party Plugin under CrossCore Embedded Studio
    • External Configuration tool in CCES
    • FIR Decimation filter
    • FIR interpolation
    • Git-Based Version Control System in CCES
    • How can I issue multiple Pre-Build or Post-Build Commands in CrossCore Embedded Studio
    • How can I obtain the CrossCore Embedded Studio Software License Agreement?
    • How can I obtain university license for Crosscore embedded studio?
    • How do I update the Add-In version being used by my CrossCore Embedded Studio project?
    • How to use custom platform with CCES_Runner.exe Utility
    • ICE feature comparison Table
    • Importing and creating multi-core projects in CrossCore Embedded Studio
    • Instrumented Profiling Report in CCES
    • Is it possible to install both a node-locked license and a corporate domain license on the same machine?
    • Is there any restriction for defining normal-word variables in seg_dmda_nw section on SHARC+?
    • Linking driver source into project
    • MPEG-4 AAC Decoders support on the ADSP-SC573
    • Re-create system.svc
    • Reprogram On-Board Debug Agent Firmware
    • Start/Stop FLEXnet License Server via Command Line
    • Support for Parallel Builds in CrossCore Embedded Studio Audit
    • System Services and Device Drivers for CrossCore®︎ Embedded Studio Training Videos Audit
    • Using Blackfin and SHARC from the command line in CrossCore Embedded Studio
    • Using CMSIS packs from the command line in CrossCore Embedded Studio
    • What are the different types of licenses for CrossCore Embedded Studio? Audit
    • What changes are needed to build a CrossCore Embedded Studio project after moving to another directory? Audit
    • What is the current working directory for the Elfloader in CrossCore Embedded Studio Audit
    • Where can I find details of CrossCore Software and Tools Anomaly Reports? Audit
    • Which versions of CrossCore Embedded Studio (CCES) do I need to install? Audit
  • +CROSSCORE: FAQ
  • Custom debug configurations in CCES
  • +Data Member Alignment: FAQ
  • +Device Driver programming: FAQ
  • Difference between ADZS-HPUSB and ADZS-USB ICE Audit Audit
  • Difference between Debug and Release configurations
  • +Difference between Emulator and Simulator: FAQ
  • +disable prelinker: FAQ
  • DND mode in CCES
  • Does CCES have any API that can be used to build automation test platform with Python Audit
  • Does ICE-1000 supported ADSP-CM407F? Audit
  • +Driver example for Timer windowed watchdog period mode.
  • +Embedded applications: FAQ
  • +EV-21569-SOM: FAQ
  • Example code for SPORT slave trigger in ADSP-21569 Ezkit Audit Audit
  • Export console output to the desired file Audit
  • export/import CCES preferences settings
  • +EXTCLK_MODE: FAQ
  • Flash Programmer Drivers for ADSP-2183x/SC83x and ADSP-SC5xx ARM Cortex A5 Cores
  • GUL-XP board with EZkit license Audit
  • +How to access darkmode appearance in CCES?
  • +How to access stereo channels individually in the Audio_Passthrough_I2S example present in GUL BSP?
  • +How to avoid CORE0 and DEBUG: FAQ
  • How to build a specific code from single source file for a specific core?
  • +How to convert long double into string: FAQ
  • How to create library files for individual modules? Audit
  • +how to deassert Slave: FAQ
  • +How to do profiling: FAQ
  • How to obtain PCB library files for ADI processors Audit
  • How to pass arguments from command line in CCES runner
  • +How to protect shared code/ data: FAQ
  • How To remove automatically added "includes" folders in CCES project Audit
  • How to use "log10f_simd" Audit
  • How to use commands in CCES runner Audit
  • How to use Device programmer in EVAL-ADICUP360 board Audit
  • How to use optimized libraries for FFT Audit
  • +HW Accelerator and SW libraries: FAQ
  • INPUT SECTIONS & INPUT SECTIONS PIN EXCLUSIVE Audit
  • Interrupt header files along with -char-size-32 switch in Sharc Audit
  • +Interrupt Vector Table: FAQ
  • Is it possible to perform stepping into the code in CCES Runner. Audit
  • Is there a way to list symbols from library (*.dlb) file? Audit
  • Is there a way to mangle or remove internal symbols ? Audit
  • JTAG switch Interface for EV-SOMCRR-EZLITE and EV-SOMCRR-EZKIT: Audit
  • +LDF from C code: FAQ
  • +linker map file: FAQ
  • +List of Processors: FAQ
  • +Loader File: FAQ
  • +MCAPI package: FAQ
  • +node-locked license: FAQ
  • +non-blocking peek functions: FAQ
  • Optimization in ARM Audit
  • +PART_SPECIFIC_HEADERS: FAQ
  • +path variables: FAQ
  • +peripheral Error: FAQ
  • +PINT modules: FAQ
  • +PM bus: FAQ
  • +Project Explorer tree: FAQ
  • +PWM mode: FAQ
  • +quad SPI mode: FAQ
  • Reset SHARC core from ARM core using RCU in SC573 Audit
  • +RTOS for older Blackfin or older SHARC: FAQ
  • +SC-573 EZkit: FAQ
  • +SC83x-FAQ
  • +SDRAM: FAQ
  • +SHARC 21469: FAQ
  • +SHARC0: FAQ
  • +SHARC: FAQ
  • +sharing global data between cores: FAQ
  • +SigmaStudioForSHARC: FAQ
  • +SIMD code: FAQ
  • +SIMD: FAQ
  • sizeof() built-in function in BF and Sharc processors Audit
  • +SPI core mode with callback: FAQ
  • +SPI flash: FAQ
  • +SPORT API: FAQ
  • +SPORT: FAQ
  • +SRCU bit: FAQ
  • SRU and DAI routing via GUI
  • +SSLDD 2.0 and SSLDD 3.0: FAQ
  • +SSLDD 3.0: FAQ
  • +SSLDD3.0: FAQ
  • +stack overflow: FAQ
  • +Static library & IP protection: FAQ
  • Streaming Data input and output in CCES
  • +suppress assembler preprocessor warning: FAQ
  • SWD with ICE-1000
  • +system.svc: FAQ
  • TDM with both SPORT channels Audit
  • TWI Transfer using 3.0 APIs
  • +two PINT modules: FAQ
  • +TX and RX DMA Interrupts: FAQ
  • Types of Pragma usage Audit
  • +U-Law and A-Law: FAQ
  • +UART Device Driver: FAQ
  • +UART ISR Callback: FAQ
  • UART sample driver code for BF706mini Audit
  • +VisualDSP++: FAQ
  • +Wakeup processor from Hibernate: FAQ
  • +When callback occurs: FAQ
  • +word addressable program: FAQ
  • [FAQ] : FORCE CONTIGUITY Audit
  • “Peripherals view” in CCES

Using CMSIS packs from the command line in CrossCore Embedded Studio

Whilst we recommend using the CrossCore Embedded Studio GUI for your development work, there are some occasions where you may find command line access useful such as build automation. This page contains a list of frequently asked questions about command line support for the Cortex-M processor families.

How do I install CrossCore Embedded Studio from a command line?

Download the latest CCES release from https://www.analog.com/cces

Linux (Ubuntu)

CCES is officially supported for the 32-bit variants of Ubuntu 14.04 and 16.04. It may also work on other flavours of Debian but will not be officially supported.

If you are using an unsupported 64-bit OS you'll need to ensure you have support for the 32-bit architecture with the following commands:

$ sudo dpkg --add-architecture i386
$ sudo apt update

$ sudo apt install libc6:i386 libstdc++6:i386

To install, run the following command to install:

$ sudo dpkg -i ${CCES-INSTALLER}.deb

CCES will be installed to:

 /opt/analog/cces/${VERSION}/

You can uninstall CCES using the following commands:

$ sudo dpkg -r adi-cces-${VERSION}
$ sudo dpkg -P adi-cces-${VERSION}
$ sudo rm -rf /opt/analog/cces/${VERSION}

Windows

On Windows, run the following command to install:

> ./ADI_CrossCoreEmbeddedStudio-Rel${VERSION}.exe /S /V"/qn INSTALLDIR=\"${INSTALL_PATH}\""

CCES can be uninstalled via the uninstall link in the start menu, or via the control panel.

What CMSIS pack files do I need?

There are a few pack files required for development of the Cortex-M series processors.

First, to make use of the CMSIS support, you need the core ARM CMSIS support (ARM.CMSIS.4.5.0 or later).

When developing for a processor family, you'll need the device family pack (DFP) for that device family, which contains all of the configurations required to build and debug for that family of processors. For example, if developing for the ADuCM3029, you'll need the ADuCM302x device family pack (AnalogDevices.ADuCM302x_DFP.x.y.z.pack).

Additionally, if you are developing using an evaluation platform from ADI (EZ-Kit, COG, CUP) then you'll need the appropriate board support pack (BSP) for the board, which contains examples and drivers for off-chip peripherals provided on the board. For example, if you are using the EV-COG-AD3029LZ evaluation platform, then you'd need the EV-COG-AD3029 BSP (AnalogDevices.EV-COG-AD3029LZ_BSP.x.y.z.pack).

The CMSIS pack files have support for dependencies, so you should be prompted to install any missing pack files.

How do I install CMSIS pack files from the web?

To install a pack from the web, first identify the pack name by visiting https://www.keil.arm.com/devices and finding the pack you want to install. The pack name is the filename with the .pack extension on the top row of the expanded tab, but without the .pack extension. For example, the pack file for the ADuCM302x Device Family Pack is "AnalogDevices.ADuCM302x_DFP.2.0.0".

To install directly from the web, use the following command:

 ${CCES}/Eclipse/cces -nosplash -consoleLog -application com.arm.cmsis.pack.installer -installPack ${PACK_NAME}

How do I install a pack file from my local filesystem?

To install a locally downloaded pack, use the following command:

 ${CCES}/Eclipse/cces -nosplash -consoleLog -application com.arm.cmsis.pack.installer -importPack ${PACK_FILE}

How do I remove a pack file I have installed?

To remove a pack, use the following command:

 ${CCES}/Eclipse/cces -nosplash -consoleLog -application com.arm.cmsis.pack.installer -deletePack ${PACK_NAME}

How do I see what CMSIS packs are installed from a command line?

There is no command line support for determining which pack files have been installed, however the pack structures will be installed into

${CCES}/ARM/packs/AnalogDevices/ 

Where the first level directory is the pack name and the second level is the pack version e.g.

ADuCM302x_DFP/2.0.0/

On Linux, you can get a full list of pack and versions in CCES 2.7.0 with the following ls command:

$ ls /opt/analog/cces/2.7.0/ARM/packs/AnalogDevices/*
/opt/analog/cces/2.7.0/ARM/packs/AnalogDevices/ADuCM302x_DFP:
2.0.0

/opt/analog/cces/2.7.0/ARM/packs/AnalogDevices/EV-COG-AD3029LZ_BSP:
1.0.0

On Windows, you can get a full list of pack files (without versions) with the following command:

> dir C:\analog\cces\2.7.0\ARM\packs\AnalogDevices\ /ad /b
ADuCM302x_DFP
EV-COG-AD3029LZ_BSP

How do I build an existing project from the command line?

To invoke the dependency, makefile generation and build process, you need to invoke the headless builder with the following commands.

On Linux:

$ /opt/analog/cces/2.7.0/Eclipse/cces -nosplash -consoleLog -application com.analog.crosscore.headlesstools \
   -data ~/cces/cmdline/ -project ~/cces/cmdline/MyProject/ -build all

On Windows:

> C:\analog\cces\2.7.0\Eclipse\ccesc -nosplash -consoleLog -application com.analog.crosscore.headlesstools \
    -data C:/path/to/workspace -project C:/path/to/project -build all

Where:

-data is the path to the workspace you want to build from

-project is the path to your project

-build identifies the configuration to build, or "all" to build all configurations. Configuration name is case insensitive.

When a project has been built, and you haven't changed any settings or added/removed any files, you can invoke the makefiles directly from your build area.
To do this, add the code generation tools location to your path

You can also use the makefile support generated by a project build to build directly.

First, ensure the ARM/gcc-arm-embedded/bin directory in your CCES install is in the PATH environment variable.

On Linux, you can use 'export' in your script or .bashrc:

$ export PATH=${PATH}:/opt/analog/cces/2.7.0/ARM/gcc-arm-embedded/bin/

On Windows, you can use the 'set' command or the "Advanced System Settings" GUI:

> set path "%PATH%;C:\analog\cces\2.7.0\ARM\gcc-arm-embedded\bin"

Then cd into your output directory, where you can invoke the following make commands:

"make all" to perform a full build of anything that's changed since the previous build.
"make clean" to perform a clean, which deletes any temporary/generated files allowing for a full build to be carried out.

Note: If you change any project settings or add/remove files, this won't be reflected in the makefiles unless you invoke the headless builder again. You can modify the makefiles directly but they will be overwritten if the headless builder is used.

How do I create a new project from the command line?

There is currently no support to create a CMSIS project from CCES via the command line. We're looking to add this in the future.

Currently your only options are to create the project under the CCES GUI, or to write a makefile based project.

How do I debug from the command line?

Debugging from the command line involves 2 components: OpenOCD (which handles the connection to the device) and gdb (which provides the debug interface)

Invoking OpenOCD

The OpenOCD command requires two configuration files (specified with the -f switch) : one for the target (CMSIS-DAP, ICE-2000, etc) found in:

 ${CCES}/ARM/openocd/share/openocd/scripts/interface/ 

and one for the target, found in the appropriate Device Family Pack under

${CCES}/ARM/packs/AnalogDevices/${DFP}/${DFP_VERSION}/openocd/scripts/target/.


You also need to include both scripts directories (specified with the -s switch):

${CCES}/ARM/openocd/share/openocd
${CCES}/ARM/packs/AnalogDevices/${DFP}/${DFP_VERSION}/openocd/scripts


You then need to invoke OpenOCD with "-c init" and an adapter speed.

Your full openocd command will therefore look something like this:

On Linux:

$ /opt/analog/cces/2.7.0/ARM/openocd/bin/openocd \
  -f /opt/analog/cces/2.7.0/ARM/openocd/share/openocd/scripts/interface/cmsis-dap.cfg \
  -f /opt/analog/cces/2.7.0/ARM/packs/AnalogDevices/ADuCM302x_DFP/2.0.0/openocd/scripts/target/aducm3029.cfg \
  -s /opt/analog/cces/2.7.0/ARM/packs/AnalogDevices/ADuCM302x_DFP/2.0.0/openocd/scripts \
  -s /opt/analog/cces/2.7.0/ARM/openocd/share/openocd/scripts \
  -c init  -c "adapter_khz 1000"

On Windows:

C:\analog\cces\2.7.0\ARM\openocd.exe \
  -f C:\analog\cces\2.7.0\ARM\openocd\share\openocd\scripts\interface\cmsis-dap.cfg \
  -f C:\analog\cces\2.7.0\ARM\packs\AnalogDevices\ADuCM302x_DFP\2.0.0\openocd\scripts\target\aducm3029.cfg \
  -s C:\analog\cces\2.7.0\ARM\packs\AnalogDevices\ADuCM302x_DFP\2.0.0\openocd\scripts \
  -s C:\analog\cces\2.7.0\ARM\openocd\share\openocd\scripts \
  -c init  -c "adapter_khz 1000"

Connecting via GDB

First, launch gdb.

On Linux:

/opt/analog/cces/2.7.0/ARM/gcc-arm-embedded/bin/arm-none-eabi-gdb

On Windows:

C:\analog\cces\2.7.0\ARM\gcc-arm-embedded\bin\arm-none-eabi-gdb.exe

Then use the 'target' command to connect to the OpenOCD session

(gdb) target remote localhost:3333

You can then use the standard gdb commands to manipulate your debug session, such as:

'load' command to load your executable

(gdb) load /path/to/executable

'continue' command to start running your application.

(gdb) continue
Tags: microcontrollers Precision Microcontrollers aducm3029
  • Share
  • History
  • More
  • Cancel
 
Related Content
  • RE: How can I program the flash of ADuCM4050 (release version of my application) using the ICE-2000?
    ADIApproved
    Hi KdT For #1 question You can use openocd from a command line to flash a program. An example command line looks like: c:/analog/cces/2.8.3/openocd -f c:/analog/cces/2.8.3/ARM/openocd/share/openocd...
  • RE: CCES Crashing while taking user input using scanf(CCES 2.8.1, EZ-KIT SC589)
    amcl
    Hi lalit.meena I'm really sorry for the delay. Unfortunately it is not currently possible to accept input with scanf using the Eclipse IDE. We'll work to address the CrossCore Debugger issue(s). However...
  • RE: How to Flash the EVAL-ADICUP360
    amcl
    I thought it was also worth mentioning that you can use OpenOCD to flash your program(s). ${CCES}/ARM/openocd/bin/openocd -f ${CCES}/ARM/openocd/share/openocd/scripts/interface/cmsis-dap.cfg -f ${CCES...
 
Related Content
  • RE: How can I program the flash of ADuCM4050 (release version of my application) using the ICE-2000?
    ADIApproved
    Hi KdT For #1 question You can use openocd from a command line to flash a program. An example command line looks like: c:/analog/cces/2.8.3/openocd -f c:/analog/cces/2.8.3/ARM/openocd/share/openocd...
  • RE: CCES Crashing while taking user input using scanf(CCES 2.8.1, EZ-KIT SC589)
    amcl
    Hi lalit.meena I'm really sorry for the delay. Unfortunately it is not currently possible to accept input with scanf using the Eclipse IDE. We'll work to address the CrossCore Debugger issue(s). However...
  • RE: How to Flash the EVAL-ADICUP360
    amcl
    I thought it was also worth mentioning that you can use OpenOCD to flash your program(s). ${CCES}/ARM/openocd/bin/openocd -f ${CCES}/ARM/openocd/share/openocd/scripts/interface/cmsis-dap.cfg -f ${CCES...