• LiDAR Solutions
    • Motor Control Hardware Platforms
    • Speech Processing Solutions
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
    Accelerate RF Subsystem Integration with COTS SoMs and Phased Array Solutions. As building a subsystem from early prototype to full deployment is never...
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
      KCC's Quizzes AQQ301 - Counting Bicycles and Tricycles

      1. Quote of the month: " People who didn't need people needed people around to know that they were the kind of people who didn't need people" - Terry Pratchett...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Taming the AI Power Storm: Part 2 of 3 Test your...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 2: Achieving Phase Repeatability

    This article discusses a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a...

EngineerZone
EngineerZone
CrossCore Embedded Studio and Add-ins
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
CrossCore Embedded Studio and Add-ins
  • Processors & DSP
  • Software & Development Tools
  • CrossCore Embedded Studio and Add-ins
  • Cancel
CrossCore Embedded Studio and Add-ins
Documents Start/Stop FLEXnet License Server via Command Line
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • FAQ
  • +a.b silicon into a x.y silicon target: FAQ
  • +accel_xxxx: FAQ
  • +ADC & DAC in audio application: FAQ
  • Add submodule files in CCES
  • +Add version of application in loader file: FAQ
  • Add-in license: FAQ
  • +ADI_SPI_TRANSCEIVER: FAQ
  • +adi_spu_Init() API: FAQ
  • +ADSO-BF609 EZkit: FAQ
  • +ADSP-21364: FAQ
  • +ADSP-214xx: FAQ
  • +ADSP-21569 Ez-kit: FAQ
  • +ADSP-21569: FAQ
  • +ADSP-2183x:FAQ
  • +ADSP-BF609 EZKIT: FAQ
  • +ADSP-BF609: FAQ
  • +ADSP-BF707: FAQ
  • +ADSP-BF70x: FAQ
  • +ADSP-SC589: FAQ
  • +ADSP-SC58x: FAQ
  • +ADSP-SC59x: FAQs
  • +ADSP-SC5xx: FAQ
  • +ADSP-SC8xx FAQs
  • +ADSP21489: FAQ
  • +ADSP215xx: FAQ
  • +alignment pragma: FAQ
  • +ARM CORE: FAQ
  • +ARM to Sharc: FAQ
  • +avoid when a project is getting build: FAQ
  • +BF-609 Evaluation board: FAQ
  • +BF518 Processor: FAQ
  • +BF703: FAQ
  • +BF706 EZ-KIT: FAQ
  • +BF706: FAQ
  • +BF706mini BSP project: FAQ
  • +BF707 SPI: FAQ
  • BITEXP and BITRET for ADSP-214xx
  • C and C++ standard library in CCES?
  • +C source file: FAQ
  • +C++ code: FAQ
  • +C-code ISRs: FAQ
  • cache invalidation and cache flushing
  • +Callback function: FAQ
  • +Calling Library Functions: FAQ
  • +cc1138: FAQ
  • +CCES: FAQ's
  • +cldp: FAQ
  • Clip double precision floating-point in C Audit
  • +CLKIN: FAQ
  • +Code folding in CCES: FAQ
  • +Configuring the Loader, Linker and Archiver: FAQ
  • +connect to the Blackfin: FAQ
  • Create Library files for individual modules Audit
  • Creating and Linking a .dlb in CCES
  • -CrossCore Embedded Studio STDIO: FAQ
    • "DO_CYCLE_COUNTS" macro in CCES
    • Build Configuration settings in CCES
    • Cache settings on SHARC-FX
    • CCES Debug configuration settings
    • CCES_HOME Environment variable
    • Change output directory path of DXE. Audit
    • Compare EV-SOMCRR-EZKIT and EV-SOMCRR-EZLITE
    • Create ASM project in CCES
    • CrossCore Embedded Studio STDIO is slow, and interrupts processing of real world data Audit
    • Default qualifier for the output sections
    • Does CrossCore Embedded Studio have a floating license option?
    • Does CrossCore Embedded Studio Support C++ 11?
    • Dump specific memory contents to a file in CCES
    • Encountering the following error - ‘Invalid license file. The license file may be obsolete, corrupted, missing, or read-only’
    • End of availability for Micrium Add-Ins for CrossCore Embedded Studio
    • Error "Cannot Satisfy Dependency" when installing 3rd Party Plugin under CrossCore Embedded Studio
    • External Configuration tool in CCES
    • FIR Decimation filter
    • FIR interpolation
    • Git-Based Version Control System in CCES
    • How can I issue multiple Pre-Build or Post-Build Commands in CrossCore Embedded Studio
    • How can I obtain the CrossCore Embedded Studio Software License Agreement?
    • How can I obtain university license for Crosscore embedded studio?
    • How do I update the Add-In version being used by my CrossCore Embedded Studio project?
    • How to use custom platform with CCES_Runner.exe Utility
    • ICE feature comparison Table
    • Importing and creating multi-core projects in CrossCore Embedded Studio
    • Instrumented Profiling Report in CCES
    • Is it possible to install both a node-locked license and a corporate domain license on the same machine?
    • Is there any restriction for defining normal-word variables in seg_dmda_nw section on SHARC+?
    • Linking driver source into project
    • MPEG-4 AAC Decoders support on the ADSP-SC573
    • Re-create system.svc
    • Reprogram On-Board Debug Agent Firmware
    • Start/Stop FLEXnet License Server via Command Line
    • Support for Parallel Builds in CrossCore Embedded Studio Audit
    • System Services and Device Drivers for CrossCore®︎ Embedded Studio Training Videos Audit
    • Using Blackfin and SHARC from the command line in CrossCore Embedded Studio
    • Using CMSIS packs from the command line in CrossCore Embedded Studio
    • What are the different types of licenses for CrossCore Embedded Studio? Audit
    • What changes are needed to build a CrossCore Embedded Studio project after moving to another directory? Audit
    • What is the current working directory for the Elfloader in CrossCore Embedded Studio Audit
    • Where can I find details of CrossCore Software and Tools Anomaly Reports? Audit
    • Which versions of CrossCore Embedded Studio (CCES) do I need to install? Audit
  • +CROSSCORE: FAQ
  • Custom debug configurations in CCES
  • +Data Member Alignment: FAQ
  • +Device Driver programming: FAQ
  • Difference between ADZS-HPUSB and ADZS-USB ICE Audit Audit
  • Difference between Debug and Release configurations
  • +Difference between Emulator and Simulator: FAQ
  • +disable prelinker: FAQ
  • DND mode in CCES
  • Does CCES have any API that can be used to build automation test platform with Python Audit
  • Does ICE-1000 supported ADSP-CM407F? Audit
  • +Driver example for Timer windowed watchdog period mode.
  • +Embedded applications: FAQ
  • +EV-21569-SOM: FAQ
  • Example code for SPORT slave trigger in ADSP-21569 Ezkit Audit Audit
  • Export console output to the desired file Audit
  • export/import CCES preferences settings
  • +EXTCLK_MODE: FAQ
  • Flash Programmer Drivers for ADSP-2183x/SC83x and ADSP-SC5xx ARM Cortex A5 Cores
  • GUL-XP board with EZkit license Audit
  • +How to access darkmode appearance in CCES?
  • +How to access stereo channels individually in the Audio_Passthrough_I2S example present in GUL BSP?
  • +How to avoid CORE0 and DEBUG: FAQ
  • How to build a specific code from single source file for a specific core?
  • +How to convert long double into string: FAQ
  • How to create library files for individual modules? Audit
  • +how to deassert Slave: FAQ
  • +How to do profiling: FAQ
  • How to obtain PCB library files for ADI processors Audit
  • How to pass arguments from command line in CCES runner
  • +How to protect shared code/ data: FAQ
  • How To remove automatically added "includes" folders in CCES project Audit
  • How to use "log10f_simd" Audit
  • How to use commands in CCES runner Audit
  • How to use Device programmer in EVAL-ADICUP360 board Audit
  • How to use optimized libraries for FFT Audit
  • +HW Accelerator and SW libraries: FAQ
  • INPUT SECTIONS & INPUT SECTIONS PIN EXCLUSIVE Audit
  • Interrupt header files along with -char-size-32 switch in Sharc Audit
  • +Interrupt Vector Table: FAQ
  • Is it possible to perform stepping into the code in CCES Runner. Audit
  • Is there a way to list symbols from library (*.dlb) file? Audit
  • Is there a way to mangle or remove internal symbols ? Audit
  • JTAG switch Interface for EV-SOMCRR-EZLITE and EV-SOMCRR-EZKIT: Audit
  • +LDF from C code: FAQ
  • +linker map file: FAQ
  • +List of Processors: FAQ
  • +Loader File: FAQ
  • +MCAPI package: FAQ
  • +node-locked license: FAQ
  • +non-blocking peek functions: FAQ
  • Optimization in ARM Audit
  • +PART_SPECIFIC_HEADERS: FAQ
  • +path variables: FAQ
  • +peripheral Error: FAQ
  • +PINT modules: FAQ
  • +PM bus: FAQ
  • +Project Explorer tree: FAQ
  • +PWM mode: FAQ
  • +quad SPI mode: FAQ
  • Reset SHARC core from ARM core using RCU in SC573 Audit
  • +RTOS for older Blackfin or older SHARC: FAQ
  • +SC-573 EZkit: FAQ
  • +SC83x-FAQ
  • +SDRAM: FAQ
  • +SHARC 21469: FAQ
  • +SHARC0: FAQ
  • +SHARC: FAQ
  • +sharing global data between cores: FAQ
  • +SigmaStudioForSHARC: FAQ
  • +SIMD code: FAQ
  • +SIMD: FAQ
  • sizeof() built-in function in BF and Sharc processors Audit
  • +SPI core mode with callback: FAQ
  • +SPI flash: FAQ
  • +SPORT API: FAQ
  • +SPORT: FAQ
  • +SRCU bit: FAQ
  • SRU and DAI routing via GUI
  • +SSLDD 2.0 and SSLDD 3.0: FAQ
  • +SSLDD 3.0: FAQ
  • +SSLDD3.0: FAQ
  • +stack overflow: FAQ
  • +Static library & IP protection: FAQ
  • Streaming Data input and output in CCES
  • +suppress assembler preprocessor warning: FAQ
  • SWD with ICE-1000
  • +system.svc: FAQ
  • TDM with both SPORT channels Audit
  • TWI Transfer using 3.0 APIs
  • +two PINT modules: FAQ
  • +TX and RX DMA Interrupts: FAQ
  • Types of Pragma usage Audit
  • +U-Law and A-Law: FAQ
  • +UART Device Driver: FAQ
  • +UART ISR Callback: FAQ
  • UART sample driver code for BF706mini Audit
  • +VisualDSP++: FAQ
  • +Wakeup processor from Hibernate: FAQ
  • +When callback occurs: FAQ
  • +word addressable program: FAQ
  • [FAQ] : FORCE CONTIGUITY Audit
  • “Peripherals view” in CCES

Start/Stop FLEXnet License Server via Command Line

Question:
Is there any way to Start/Stop LMTOOLS from command line?

Answer:
Yes. Start lmgrd as an application from a Windows command shell using the following syntax:
C:\flexlm> lmgrd -c license_file_list -L [+]debug_log_path
Where,
• license_file_list is one or more of the following:
- the full path to a single license file
- a directory, where all files named *.lic in that directory are used

• debug_log_path is the full path to the debug log file
Prepending debug_log_path with the + character appends logging entries

We recommend referring to the chapter "Starting the License Server Manager on Windows" in the attached FLEXnet Licensing End User Guide. This section provides detailed instructions on how to manually start the license server from the command line.
And, the lmdown utility through lmutil.exe allows for the graceful shutdown of selected license daemons (both lmgrd and selected vendor daemons) on all machines.
To view the available command-line options, you can run the following command from your LMSERVER installation directory:
lmutil.exe lmdown -help

PDF