Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC Quiz AQQ299 about Opamp open looop gain and LTspice (a kind proposal from Al Butvidas)

      1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits next to you and says 'wasn't that...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Understanding Voltage Domain Isolation in Field-Bus...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

EngineerZone
EngineerZone
CrossCore Embedded Studio and Add-ins
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
CrossCore Embedded Studio and Add-ins
  • Processors & DSP
  • Software & Development Tools
  • CrossCore Embedded Studio and Add-ins
  • Cancel
CrossCore Embedded Studio and Add-ins
Documents ADSP-SC835/21835 SHARC FX and ADSP-SC594 Family Cortex A5 Custom Flash Drivers
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • FAQ
  • +a.b silicon into a x.y silicon target: FAQ
  • +accel_xxxx: FAQ
  • +ADC & DAC in audio application: FAQ
  • Add submodule files in CCES
  • +Add version of application in loader file: FAQ
  • Add-in license: FAQ
  • +ADI_SPI_TRANSCEIVER: FAQ
  • +adi_spu_Init() API: FAQ
  • +ADSO-BF609 EZkit: FAQ
  • +ADSP-21364: FAQ
  • +ADSP-214xx: FAQ
  • +ADSP-21569 Ez-kit: FAQ
  • +ADSP-21569: FAQ
  • +ADSP-BF609 EZKIT: FAQ
  • +ADSP-BF609: FAQ
  • +ADSP-BF707: FAQ
  • +ADSP-BF70x: FAQ
  • +ADSP-SC589: FAQ
  • +ADSP-SC58x: FAQ
  • +ADSP-SC59x: FAQs
  • +ADSP-SC5xx: FAQ
  • +ADSP-SC8xx FAQs
  • +ADSP21489: FAQ
  • +ADSP215xx: FAQ
  • +alignment pragma: FAQ
  • +ARM CORE: FAQ
  • +ARM to Sharc: FAQ
  • +avoid when a project is getting build: FAQ
  • +BF-609 Evaluation board: FAQ
  • +BF518 Processor: FAQ
  • +BF703: FAQ
  • +BF706 EZ-KIT: FAQ
  • +BF706: FAQ
  • +BF706mini BSP project: FAQ
  • +BF707 SPI: FAQ
  • BITEXP and BITRET for ADSP-214xx
  • C and C++ standard library in CCES?
  • +C source file: FAQ
  • +C++ code: FAQ
  • +C-code ISRs: FAQ
  • cache invalidation and cache flushing
  • +Callback function: FAQ
  • +Calling Library Functions: FAQ
  • +cc1138: FAQ
  • +CCES: FAQ's
  • +cldp: FAQ
  • Clip double precision floating-point in C Audit
  • +CLKIN: FAQ
  • +Code folding in CCES: FAQ
  • +Configuring the Loader, Linker and Archiver: FAQ
  • +connect to the Blackfin: FAQ
  • Create Library files for individual modules Audit
  • Creating and Linking a .dlb in CCES
  • +CrossCore Embedded Studio STDIO: FAQ
  • +CROSSCORE: FAQ
  • Custom debug configurations in CCES
  • +Data Member Alignment: FAQ
  • +Device Driver programming: FAQ
  • Difference between ADZS-HPUSB and ADZS-USB ICE Audit Audit
  • Difference between Debug and Release configurations
  • +Difference between Emulator and Simulator: FAQ
  • +disable prelinker: FAQ
  • DND mode in CCES
  • Does CCES have any API that can be used to build automation test platform with Python Audit
  • Does ICE-1000 supported ADSP-CM407F? Audit
  • +Driver example for Timer windowed watchdog period mode.
  • +Embedded applications: FAQ
  • +EV-21569-SOM: FAQ
  • Example code for SPORT slave trigger in ADSP-21569 Ezkit Audit Audit
  • Export console output to the desired file Audit
  • export/import CCES preferences settings
  • +EXTCLK_MODE: FAQ
  • Flash Programmer Drivers for ADSP-2183x/SC83x and ADSP-SC5xx ARM Cortex A5 Cores
  • GUL-XP board with EZkit license Audit
  • +How to access darkmode appearance in CCES?
  • +How to access stereo channels individually in the Audio_Passthrough_I2S example present in GUL BSP?
  • +How to avoid CORE0 and DEBUG: FAQ
  • How to build a specific code from single source file for a specific core?
  • +How to convert long double into string: FAQ
  • How to create library files for individual modules? Audit
  • +how to deassert Slave: FAQ
  • +How to do profiling: FAQ
  • How to obtain PCB library files for ADI processors Audit
  • How to pass arguments from command line in CCES runner
  • +How to protect shared code/ data: FAQ
  • How To remove automatically added "includes" folders in CCES project Audit
  • How to use "log10f_simd" Audit
  • How to use commands in CCES runner Audit
  • How to use Device programmer in EVAL-ADICUP360 board Audit
  • How to use optimized libraries for FFT Audit
  • +HW Accelerator and SW libraries: FAQ
  • INPUT SECTIONS & INPUT SECTIONS PIN EXCLUSIVE Audit
  • Interrupt header files along with -char-size-32 switch in Sharc Audit
  • +Interrupt Vector Table: FAQ
  • Is it possible to perform stepping into the code in CCES Runner. Audit
  • Is there a way to list symbols from library (*.dlb) file? Audit
  • Is there a way to mangle or remove internal symbols ? Audit
  • JTAG switch Interface for EV-SOMCRR-EZLITE and EV-SOMCRR-EZKIT: Audit
  • +LDF from C code: FAQ
  • +linker map file: FAQ
  • +List of Processors: FAQ
  • +Loader File: FAQ
  • +MCAPI package: FAQ
  • +node-locked license: FAQ
  • +non-blocking peek functions: FAQ
  • Optimization in ARM Audit
  • +PART_SPECIFIC_HEADERS: FAQ
  • +path variables: FAQ
  • +peripheral Error: FAQ
  • +PINT modules: FAQ
  • +PM bus: FAQ
  • +Project Explorer tree: FAQ
  • +PWM mode: FAQ
  • +quad SPI mode: FAQ
  • Reset SHARC core from ARM core using RCU in SC573 Audit
  • +RTOS for older Blackfin or older SHARC: FAQ
  • +SC-573 EZkit: FAQ
  • +SC83x-FAQ
  • +SDRAM: FAQ
  • +SHARC 21469: FAQ
  • +SHARC0: FAQ
  • +SHARC: FAQ
  • +sharing global data between cores: FAQ
  • +SigmaStudioForSHARC: FAQ
  • +SIMD code: FAQ
  • +SIMD: FAQ
  • sizeof() built-in function in BF and Sharc processors Audit
  • +SPI core mode with callback: FAQ
  • -SPI flash: FAQ
    • ADSP-SC835/21835 SHARC FX and ADSP-SC594 Family Cortex A5 Custom Flash Drivers
    • SPI flash communication using DMA Audit
    • SPI Flash Read-Back in ADSP-21593
  • +SPORT API: FAQ
  • +SPORT: FAQ
  • +SRCU bit: FAQ
  • SRU and DAI routing via GUI
  • +SSLDD 2.0 and SSLDD 3.0: FAQ
  • +SSLDD 3.0: FAQ
  • +SSLDD3.0: FAQ
  • +stack overflow: FAQ
  • +Static library & IP protection: FAQ
  • Streaming Data input and output in CCES
  • +suppress assembler preprocessor warning: FAQ
  • SWD with ICE-1000
  • +system.svc: FAQ
  • TDM with both SPORT channels Audit
  • TWI Transfer using 3.0 APIs
  • +two PINT modules: FAQ
  • +TX and RX DMA Interrupts: FAQ
  • Types of Pragma usage Audit
  • +U-Law and A-Law: FAQ
  • +UART Device Driver: FAQ
  • +UART ISR Callback: FAQ
  • UART sample driver code for BF706mini Audit
  • +VisualDSP++: FAQ
  • +Wakeup processor from Hibernate: FAQ
  • +When callback occurs: FAQ
  • +word addressable program: FAQ
  • [FAQ] : FORCE CONTIGUITY Audit
  • “Peripherals view” in CCES

ADSP-SC835/21835 SHARC FX and ADSP-SC594 Family Cortex A5 Custom Flash Drivers

The following documentation explains how to create custom flash target side algorithms for the ADSP-SC835/21835 SHARC FX core as well as the ADSP-SC594 Family Cortex A5 core. This documentation refers to a setup with CrossCore Embedded Studio (CCES) version 3.0.2.

Import Algorithm Project

  • Launch CCES and import the project with the correct device that the algorithm is being developed for. Please name target side algorithm project appropriately. A project can be created from scratch but it is highly recommended to import one of the projects provided and modify if necessary.
  • After the project has been imported, a major component of the algorithm generation is making sure the final compiled application contains contiguous memory locations. In order to accomplish this, we need to verify the memory sections so that all valid areas in the application are within the same section. The screenshot below is an example for the SHARC-FX of placing all areas into the L2_ram section to maintain contiguous memory locations.

  • If the application is not all in contiguous memory the following must take place:
    • For SHARC-FX, select the system.svc file and navigate to the "Startup Code/LSP" tab and place any non default populated sections into L2 ram.
    • For ARM projects, select the system.svc file and navigate to the "Heap and Stack" tab in order to customize the system heap to 16kB (suggested) to ensure the heap can fit into the algorithm project. Next, navigate to the "Linker Files" folder to change the target memory for code and data to L2. The L2 region has been the default for algorithm projects and matches up with the working area for all openOCD support. Lastly once the system.svc is saved the the linker scripts have been generated, find the "app.ld" file in the "system/linker" folder. Open in a text editor and similar to the SHARC-FX make sure that all non default populated sections into "MEM_L2_CACHED". The entries may need to be updated as well. Below is an example of a possible change...

/* Abort mode stack */
.stack_abort (NOLOAD) :
{
    __stack_abort_end = . ;
    KEEP(*(.stack_abort))
    __stack_abort_start = . ;
} > MEM_L2_CACHED = 0
        

               would be change to...

/* Abort mode stack */
.stack_abort :
{
    __stack_abort_start = . ;
    KEEP(*(.stack_abort))
    __stack_abort_end = . ;
} > MEM_L2_CACHED

                Lastly, navigate to the "app_heap_stack.c" file in the system/heap_stack folder and open in a text editor. To ensure that all information is stored in contiguous memory and the same program headers, the object entries under the definitions need to be updated accordingly...

/* The object used for the system heap. */
uint8_t __adi_heap_object[__ADI_SYSTEM_HEAP_SIZE * __ADI_SYSTEM_HEAP_SIZE_UNITS]
        __attribute__ ((aligned (__ADI_SYSTEM_HEAP_ALIGN)))
        __attribute__ ((section (".heap,\"aw\",%nobits //")));

               would be change to...

/* The object used for the system heap. */
uint8_t __adi_heap_object[__ADI_SYSTEM_HEAP_SIZE * __ADI_SYSTEM_HEAP_SIZE_UNITS]
        __attribute__ ((aligned (__ADI_SYSTEM_HEAP_ALIGN)))
        __attribute__ ((section (".heap")));

               This would be done for all corresponding entries in the "app_heap_stack.c" file.

To ensure the memory locations are all correct, generate and reference the *.map.xml to validate memory locations for all areas. Map files may not be generated by default. To enable map file generation go into the Project Properties → C/C++ Build → Settings and under the Tool Settings tab select General under the CrossCore SHARC-FX C Linker (or linker specific to your project) section. Here there should be a checkbox to generate symbol map.

 

If any areas that may be accessed are not included in the memory organization, please add them to avoid any access violations.

  • Within the system.svc, ensure that the SPI driver is included in the project generation. The "Pin Multiplexing" may differ depending on the SPI peripheral selection and setup. The Pin Multiplexing used for the standard 2183x_flash example is based on the  ADSP-21835W-EV-SOM evaluation board. This board uses the SPI1 peripheral in single SPI mode using CLK, D2, D3, MISO, MOSI and SS selections. D2 and D3 might not be necessary in single SPI mode however. Based on the custom board configuration, this should be checked and updated accordingly. Below is a screenshot of the example Pin Multiplexing page within system.svc.

Update source files if necessary

  • Now that the project is generated and all areas of memory are set up, the algorithm development can be started. Update the main.c and main.h files with any additional information for the custom algorithm. The default main.c and main.h should work for standard ADI evaluation boards with their corresponding processors and external flash devices.

Essentials for the target side algorithm main.c

  • The external flash device will differ depending on the user's setup. For example, the ADSP21835W-EV-SOM is connected via SPI to the IS25LP512M external flash device by default. This external flash contains a unique manufacturer and device id that are identified in main.c as shown below

/* Chip info (for IS25LP512M) */
#define MANUF_ID                0x9D
#define DEVICE_ID               0x601A

  • The IS25LP512M external flash also contains specific flash commands. The flash commands will depend on the external flash that is being used with the customer's setup and could vary. Below is the example code in main.c for the IS25LP512M flash commands. As the comment suggests, refer to the corresponding data sheet for the flash commands on a specific flash chip

IS25LP512M flash commands

/* Select SPI Flash Commands (from ISSI IS25LP512M, 512-MBit serial flash device data sheet) */
#define CMD_RESET_ENABLE        0x66u
#define CMD_RESET_DEVICE        0x99u

#define CMD_SR1_READ            0x05u

#define CMD_SR1_WRITE           0x01u

#define CMD_JEDEC_READ          0x9fu
#define CMD_SECTOR_ERASE        0x20u
#define CMD_BLOCK_ERASE         0xD8u
#define CMD_WRITE_ENABLE        0x06u
#define CMD_SINGLE_MODE_WRITE   0x02u
#define CMD_SINGLE_MODE_READ    0x03u
#define CMD_SINGLE_FAST_READ    0x13u
#define CMD_ENABLE_RESET        0x66u
#define CMD_RESET_DEVICE        0x99u

#define CMD_CHIP_ERASE          0xC7u

flash_commands_t

typedef enum {
	CMD_NO_ACTION = 0,
	CMD_READ = 1,
	CMD_PROGRAM = 2,
	CMD_LOCK = 3,
	CMD_ERASE_ALL = 4,
	CMD_ERASE_SECTOR = 5,
	CMD_READID = 6,
} flash_commands_t;

  • The flash_commands_t enum indicates the commands that will be available for execution. It is highly recommended not to change or add any commands as these directly relate to command numbers used in OpenOCD driver support.

flash_params

struct __attribute__((__packed__)) flash_params {
	uint32_t offset;     /* offset */
	uint32_t len;        /* Number of bytes */
	uint32_t cmd;        /* Command */
	uint32_t status;     /* Return status */
	uint32_t ready;      /* Handshake signal. Is buffer ready? */
	uint32_t device_id;  /* Device ID of flash */
	uint32_t buf_addr;   /* Address of data buffer. */
};

  • The flash_params structure is where all of the input parameters from OpenOCD are saved. This should not have to be modified unless there are some additional parameters down the road might need to be included.

flashloader_init

void flashloader_init(struct flash_params *params, uint32_t *buf1) {
	/* Initialize params buffers */
	memset((void *)params, 0, 1 * sizeof(struct flash_params));
	params[0].buf_addr = (uint32_t)buf1;
}

  • The flashloader_init function sets up the parameter structure and buffer address in memory.

Memory attributes

/* max_buffer_size is necessary for algorithm builds and post processing scripts. DO NOT optimize out */
/* Only necessary for 3.0.3 support */
uint32_t max_buffer_size = BUFFER_SIZE;

/* Flashloader parameter structure. */
__attribute__ ((section(".buffer.g_cfg")))
volatile struct flash_params g_cfg[1];

/* Data buffer 1. */ 
__attribute__ ((section(".buffer.g_buf1")))
volatile uint8_t g_buf1[BUFFER_SIZE];

  • This code portion is setting up the memory attributes for the flash parameters, data buffer and max buffer size (introduced and only necessary for CCES 3.0.3 support). We are creating the .buffer.g_cfg and .buffer.g_buf1 sections that will need to be added to the memory map in the startup/LSP. There is room for double buffering down the road, we would just need to increase the flash_params array and add .buffer.g_buf2. 

When adding the .buffer.g_cfg and .buffer.g_buf1 sections to the memory map, if the startup/LSP file is saved and generated your modifications to the memmap and ldscript files will be overwritten and will need to be modified again to have all sections in L2_ram_fx. To avoid this, it may be best to add them directly to the memmap and ldscript files. Compile and check map.xml file to ensure everything is in the right place.

Algorithm Version

/* Set the algorithm version following yy/mm/dd format */
#pragma message("Warning: Ensure the algorithm version (algo_version) is updated if any changes are made to this file.")
uint32_t algo_version = 0x240815;

  • The algorithm version is also an important aspect that should be included to be able to keep track and update any changes to the algorithm project in the future. Below is the code portion that should be included.

  • The major portion of the flash algorithm template within  main.c is the top level while loop containing the  ProcessCommand() function. Here is where we wait for the flash command provided, along with all of the input parameters provided by the user when constructing their target-side flash algorithm driver in OpenOCD. In the ProcessCommand() function, add all of the flash command cases enabled in flash_commands_t and their corresponding functions to execute the flash commands. Remember to save the result to status attribute of g_cfg so that OpenOCD side can recognize success or failure.

ProcessCommand Function

static ERROR_CODE ProcessCommand(void)
{
	int result = 0;
	uint32_t *pstatus;
	uint8_t prog_buffer[g_cfg[0].len];
	uint8_t read_buffer[g_cfg[0].len];

	switch (g_cfg[0].cmd) {
	case CMD_READ:
		result = ReadData(g_cfg[0].offset, g_cfg[0].len, 1, (int *) read_buffer, 1);
		if (result == NO_ERR)
			memcpy((uint8_t *)g_cfg[0].buf_addr, read_buffer, g_cfg[0].len);
		break;
	case CMD_PROGRAM:
		memcpy(prog_buffer, (uint8_t *)g_cfg[0].buf_addr, g_cfg[0].len);
		result = WriteData(g_cfg[0].offset, g_cfg[0].len, 1, (int *)prog_buffer, 1);
		break;

	case CMD_LOCK:
		/*
		 * Handle lock if applicable
		 * pstatus = &g_cfg[0].status;
		 */
		break;

	case CMD_ERASE_ALL:
		result = FlashChipErase();
		break;

	case CMD_ERASE_SECTOR:
		result = FlashEraseSector(g_cfg[0].offset);
		break;

	case CMD_READID:
		result = ReadDeviceID();
		if (result == NO_ERR)
			g_cfg[0].device_id = AFP_IdCode;
		break;

	default:
		/* Command not listed */
		result = UNKNOWN_COMMAND;
		break;
	}

	return result;
}

The usage of assembly breakpoints as shown below is essential during target-side algorithm development. This allows the OpenOCD target-side flash algorithm driver to recognize when the current flash command is done executing. The assembly syntax and command will vary depending architecture and instruction set that is used with the above example being for SHARC-FX.

Assembly Breakpoint Example

// Halt to read status and detect error during algorithm initialization
asm("BREAK.N 0;")

  • Once the development is complete for the target-side algorithm, build and retrieve the resultant binary file that should be located in the corresponding build configuration folder (typically "Debug" or "Release"). This binary file can be used directly with the -driver switch in cldp

Debug Use

  • Like any other application, the algorithm project created can be debugged and stepped through to ensure that the custom algorithm project is behaving as intended. To do so, comment out the #define ASM_HALT in the main.h file to make sure the assembly breakpoints are not hit.
  • From there, the user can start a normal debug session to run until main and proceed to the main while loop looking for g_cfg[0].ready == BUFFER_EMPTY. This is where the user can manipulate the g_cfg[0] structure variable in a watch list to input any necessary parameters that would be tested. For example, modifying the g.ready to 0xFFFFFFFF, the g.cmd to 0x4 would allow the start of a mass erase command to execute. Stepping through or running to make sure that the g.status attribute of the structure remains 0x0 for success. This process can be handled for any commands that wish to be tested with the addition of any necessary parameters.
  • Please note that it is essential to uncomment #define ASM_HALT before rebuilding the algorithm binary. This is necessary for running the algorithm successfully outside of a debug environment.

Board and algorithm .cfg file hierarchy

  • The current process utilizes three files to accurately set up the flash banks for each memory supported; the board file, the specific memory file and the algo finder file.

Board File

  • The top level of the hierarchy is the board file where generally any information regarding board setups are present. Please note that board files are separate from target files. Below is an updated snippet of adsp21835w_ev_som.cfg. The flash bank parameters for each memory region supported are filled in via the specific memory regions .cfg file. Definitions for enabling different memory regions has been included, however, it is recommended not to disable memory regions for standard board files. 

adsp21835w_ev_som.cfg snippet

if { $ENABLE_SPI_FLASH == 1 } {
    # Find and set up SPI flash algorithm parameters
    source [find board/flash_algorithms/issi25lp512m.cfg]
    set SPI_FLASH_ALGO_FILENAME 2183x_flash.inc
    set SPI_FLASH_PARAMETER_FILENAME 2183x_flash_params.inc
    set_algo_paths $SPI_FLASH_ALGO_FILENAME $SPI_FLASH_PARAMETER_FILENAME
 
    flash bank $_CHIPNAME.spi adsp2183x $_FLASH_BASE $_FLASH_SIZE 0 0 $_TARGETNAME_SFX $_FLASH_SECTOR_SIZE $ALGO_PATH $PARAMETER_PATH
}

  • The flash bank name ("$_CHIPNAME.spi" in this case) is extremely important especially when planning to use support with CCES. The names are what allow CCES to recognize how and what flash banks are available to compare to the xml for a specific processor selected.
  • The location of all board files will reside in <CCES_PATH>\3.0.2\ARM\openocd\share\scripts\board

Specific Memory File

  • The second level of the hierarchy is the specific memory file. This could include a different number of memory types such as SPI, xSPI hyperflash, xSPI NOR flash, etc. The main purpose of this file is to create the algorithm file and algorithm parameter file variables for flash bank usage. Below is an example of the issi25lp512m.cfg that supports SPI flash for the ADSP-SC83x SOM board. These files can be changed, updated, or created based on the specific .inc algorithm and params file included.

ISSI25LP512M.cfg

# SPDX-License-Identifier: GPL-2.0-or-later
# Copyright (c) 2024 Analog Devices, Inc.
 
# Set flash parameters
set _FLASH_BASE 0x0
set _FLASH_SIZE 0x4000000
set _FLASH_SECTOR_SIZE 0x10000
 
proc set_algo_paths { inc_file param_file } {
    global ALGO_PATH PARAMETER_PATH
 
    source [find board/flash_algorithms/algoFileFinder.cfg]
 
    # Find and set the ALGO_PATH
    set ALGO_PATH [findAndSetFile $scriptDirectory $inc_file]
    if { [string length $ALGO_PATH] <= 0} {
        set ALGO_PATH $inc_file
        echo "Could not find $inc_file in [file dirname [info script]]"
    }
 
    # Find and set PARAMETER_PATH
    set PARAMETER_PATH [findAndSetFile $scriptDirectory $param_file]
    if { [string length $PARAMETER_PATH] <= 0} {
        set PARAMETER_PATH $param_file
        echo "Could not find $param_file in [file dirname [info script]]"
    }
}

  • The location of all specific memory files will reside in "<CCES_PATH>\3.0.2\ARM\openocd\share\openocd\board\flash_algorithms"

Algo Finder File

  • This helper file is a simple routine to search for the specified files in order to successfully set up variables for the flash bank parameters. This file should not be modified and is simply a helper file for shared functionality used by specific memory files in the second layer.

algoFileFinder.cfg

# Copyright (c) 2024 Analog Devices, Inc. All Rights Reserved.
# This software is proprietary to Analog Devices, Inc. and its licensors.
 
# Define a procedure to find and set the file path
proc findAndSetFile {directory pattern} {
    set files [glob -nocomplain -directory $directory $pattern]
 
    if {[llength $files] > 0} {
        return [lindex $files 0]
    } else {
        return ""
    }
}
 
# Get the directory of the current script
set scriptDirectory [file dirname [info script]]

  • Please note, this process slightly differs for ARM and other non SHARC-FX architectures, primarily with project generation and handling of the linker scripts with memory allocation. For any questions, please contact Analog Devices support team to provide additional information and references.
  • The location of the algo finder file will reside in "<CCES_PATH>\3.0.2\ARM\openocd\share\openocd\board\flash_algorithms"

Cldp.exe usage

  • The included command line switches are also necessary when running cldp:
    • -board customBoardFile.cfg
    • -driver <PATH_TO_FLASH_DRIVER> (flash driver is what was created earlier in this document)
  • More information on the above additional switches can be found in the CCES 3.0.2 Release Notes.
  • Here are some command line examples for an ADSP-SC83x/ADSP-2183x SHARC-FX cores and SC594 ARM, respectively...
    • cldp.exe -proc ADSP-21835 -emu 2000 -driver "<PATH_TO_FLASH_DRIVER>" -board customBoardFile.cfg -cmd prog -file "program.ldr"
    • cldp.exe -proc ADSP-SC594 -emu 2000 -core 0 -driver "<PATH_TO_FLASH_DRIVER>" -board customBoardFile.cfg -cmd prog -file "program.ldr"

3542.target_side_algo_examples.zip

Tags: Audio Signal Processors ADSP-SC594 ADSP-21835 SHARC Audio Processors/SoCs