Question:
UART loopback example in FreeRTOS for ADSP-SC594.
Answer:
This example code demonstrates a UART loopback between UART1 and UART2 in FreeRTOS environment.
To test the project, connect the UART1_TX pin to the UART2_RX pin. You can verify the output using the Tera Term application by connecting a P3 C-type USB cable from the SC-594 SOM to your PC. In Tera Term application set the baud rate to 115200 .