Question:
Example project for TWI data transfer between TWI1 and TWI0 in ADSP-BF609
Answer:
In the attached project, TWI1 sends 20 datas to TWI0 in ADSP-BF609 EZKIT. Below are the hardware connections are required to do data transfer between TWI1 to TWI0.
In P1A port, Please make the following hardware connections
TWI0_SCL-79 ------> TWI1_SCL-42
TWI0_SDA-80 ------> TWI1_SDA-41