Power Integrity for High Performance Measurement Systems

    Increasing data rates driven by AI workloads and the evolution from 5G to emerging 6G standards are placing new demands on electronic test and measurement...
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
      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read the Blog:  Simplified I/O: One Chip, Flexible Voltage Output, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Simplified I/O: One Chip, Flexible Voltage Outpu...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

EngineerZone
EngineerZone
CrossCore Embedded Studio and Add-ins
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
CrossCore Embedded Studio and Add-ins
  • Processors & DSP
  • Software & Development Tools
  • CrossCore Embedded Studio and Add-ins
  • Cancel
CrossCore Embedded Studio and Add-ins
Documents Single interrupt block for both rising and falling edges in ADSP-21569
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • FAQ
  • +a.b silicon into a x.y silicon target: FAQ
  • +accel_xxxx: FAQ
  • +ADC & DAC in audio application: FAQ
  • Add submodule files in CCES
  • +Add version of application in loader file: FAQ
  • Add-in license: FAQ
  • +ADI_SPI_TRANSCEIVER: FAQ
  • +adi_spu_Init() API: FAQ
  • +ADSO-BF609 EZkit: FAQ
  • +ADSP-21364: FAQ
  • +ADSP-214xx: FAQ
  • +ADSP-21569 Ez-kit: FAQ
  • -ADSP-21569: FAQ
    • ADSP-21569 SPI Core mode Sample Project Audit
    • ASRC I2S Audio pass through code for ADSP-21569 Audit
    • Configure SPI Target as a Transmitter
    • Sample based talk through code for Stereo mode in ADSP-21569 EZ-KIT Audit
    • Sample based talk through code for TDM4 mode in ADSP-21569 EZ-KIT Audit
    • Single interrupt block for both rising and falling edges in ADSP-21569
  • +ADSP-2183x:FAQ
  • +ADSP-BF609 EZKIT: FAQ
  • +ADSP-BF609: FAQ
  • +ADSP-BF707: FAQ
  • +ADSP-BF70x: FAQ
  • +ADSP-SC589: FAQ
  • +ADSP-SC58x: FAQ
  • +ADSP-SC59x: FAQs
  • +ADSP-SC5xx: FAQ
  • +ADSP-SC8xx FAQs
  • +ADSP21489: FAQ
  • +ADSP215xx: FAQ
  • +alignment pragma: FAQ
  • +ARM CORE: FAQ
  • +ARM to Sharc: FAQ
  • +avoid when a project is getting build: FAQ
  • +BF-609 Evaluation board: FAQ
  • +BF518 Processor: FAQ
  • +BF703: FAQ
  • +BF706 EZ-KIT: FAQ
  • +BF706: FAQ
  • +BF706mini BSP project: FAQ
  • +BF707 SPI: FAQ
  • BITEXP and BITRET for ADSP-214xx
  • C and C++ standard library in CCES?
  • +C source file: FAQ
  • +C++ code: FAQ
  • +C-code ISRs: FAQ
  • cache invalidation and cache flushing
  • +Callback function: FAQ
  • +Calling Library Functions: FAQ
  • +cc1138: FAQ
  • +CCES: FAQ's
  • +cldp: FAQ
  • Clip double precision floating-point in C Audit
  • +CLKIN: FAQ
  • +Code folding in CCES: FAQ
  • +Configuring the Loader, Linker and Archiver: FAQ
  • +connect to the Blackfin: FAQ
  • Create Library files for individual modules Audit
  • Creating and Linking a .dlb in CCES
  • +CrossCore Embedded Studio STDIO: FAQ
  • +CROSSCORE: FAQ
  • Custom debug configurations in CCES
  • +Data Member Alignment: FAQ
  • +Device Driver programming: FAQ
  • Difference between ADZS-HPUSB and ADZS-USB ICE Audit Audit
  • Difference between Debug and Release configurations
  • +Difference between Emulator and Simulator: FAQ
  • +disable prelinker: FAQ
  • DND mode in CCES
  • Does CCES have any API that can be used to build automation test platform with Python Audit
  • Does ICE-1000 supported ADSP-CM407F? Audit
  • +Driver example for Timer windowed watchdog period mode.
  • +Embedded applications: FAQ
  • +EV-21569-SOM: FAQ
  • Example code for SPORT slave trigger in ADSP-21569 Ezkit Audit Audit
  • Export console output to the desired file Audit
  • export/import CCES preferences settings
  • +EXTCLK_MODE: FAQ
  • Flash Programmer Drivers for ADSP-2183x/SC83x and ADSP-SC5xx ARM Cortex A5 Cores
  • GUL-XP board with EZkit license Audit
  • +How to access darkmode appearance in CCES?
  • +How to access stereo channels individually in the Audio_Passthrough_I2S example present in GUL BSP?
  • +How to avoid CORE0 and DEBUG: FAQ
  • How to build a specific code from single source file for a specific core?
  • +How to convert long double into string: FAQ
  • How to create library files for individual modules? Audit
  • +how to deassert Slave: FAQ
  • +How to do profiling: FAQ
  • How to obtain PCB library files for ADI processors Audit
  • How to pass arguments from command line in CCES runner
  • +How to protect shared code/ data: FAQ
  • How To remove automatically added "includes" folders in CCES project Audit
  • How to use "log10f_simd" Audit
  • How to use commands in CCES runner Audit
  • How to use Device programmer in EVAL-ADICUP360 board Audit
  • How to use optimized libraries for FFT Audit
  • +HW Accelerator and SW libraries: FAQ
  • INPUT SECTIONS & INPUT SECTIONS PIN EXCLUSIVE Audit
  • Interrupt header files along with -char-size-32 switch in Sharc Audit
  • +Interrupt Vector Table: FAQ
  • Is it possible to perform stepping into the code in CCES Runner. Audit
  • Is there a way to list symbols from library (*.dlb) file? Audit
  • Is there a way to mangle or remove internal symbols ? Audit
  • JTAG switch Interface for EV-SOMCRR-EZLITE and EV-SOMCRR-EZKIT: Audit
  • +LDF from C code: FAQ
  • +linker map file: FAQ
  • +List of Processors: FAQ
  • +Loader File: FAQ
  • +MCAPI package: FAQ
  • +node-locked license: FAQ
  • +non-blocking peek functions: FAQ
  • Optimization in ARM Audit
  • +PART_SPECIFIC_HEADERS: FAQ
  • +path variables: FAQ
  • +peripheral Error: FAQ
  • +PINT modules: FAQ
  • +PM bus: FAQ
  • +Project Explorer tree: FAQ
  • +PWM mode: FAQ
  • +quad SPI mode: FAQ
  • Reset SHARC core from ARM core using RCU in SC573 Audit
  • +RTOS for older Blackfin or older SHARC: FAQ
  • +SC-573 EZkit: FAQ
  • +SC83x-FAQ
  • +SDRAM: FAQ
  • +SHARC 21469: FAQ
  • +SHARC0: FAQ
  • +SHARC: FAQ
  • +sharing global data between cores: FAQ
  • +SigmaStudioForSHARC: FAQ
  • +SIMD code: FAQ
  • +SIMD: FAQ
  • sizeof() built-in function in BF and Sharc processors Audit
  • +SPI core mode with callback: FAQ
  • +SPI flash: FAQ
  • +SPORT API: FAQ
  • +SPORT: FAQ
  • +SRCU bit: FAQ
  • SRU and DAI routing via GUI
  • +SSLDD 2.0 and SSLDD 3.0: FAQ
  • +SSLDD 3.0: FAQ
  • +SSLDD3.0: FAQ
  • +stack overflow: FAQ
  • +Static library & IP protection: FAQ
  • Streaming Data input and output in CCES
  • +suppress assembler preprocessor warning: FAQ
  • SWD with ICE-1000
  • +system.svc: FAQ
  • TDM with both SPORT channels Audit
  • TWI Transfer using 3.0 APIs
  • +two PINT modules: FAQ
  • +TX and RX DMA Interrupts: FAQ
  • Types of Pragma usage Audit
  • +U-Law and A-Law: FAQ
  • +UART Device Driver: FAQ
  • +UART ISR Callback: FAQ
  • UART sample driver code for BF706mini Audit
  • +VisualDSP++: FAQ
  • +Wakeup processor from Hibernate: FAQ
  • +When callback occurs: FAQ
  • +word addressable program: FAQ
  • [FAQ] : FORCE CONTIGUITY Audit
  • “Peripherals view” in CCES

Single interrupt block for both rising and falling edges in ADSP-21569

Question:
Single interrupt block for both rising and falling edges in ADSP-21569

Answer:
The attached example is used to configure interrupt block1 raises the interrupt for both falling and raising edges of the push button connected in portC.

6114.PushButton.zip

Tags: ADSP-21569 Audio Signal Processors SHARC Audio Processors/SoCs
  • Share
  • History
  • More