Question:
Is SSLDD 3.0 support ADSP-SC58x and ADSP-SC57x processor families?
Answer:
Yes. SSLDD 3.0 support for ADSP-SC5xx (1.0.0) add-in adds "SSLDD_3_SUPPORT_FOR_SC5xx" to pre-processor definitions of the project which enables the inclusion of SSLDD v3.0 source for ADSP-SC58x and ADSP-SC57x processors. It also adds PDMA service to the project which is required for some of the modules.
The below list of modules have SSLDD 3.0 support for ADSP-SC58x and ADSP-SC57x processors in CCES 2.9.1 release
• SPI
• TWI
• SPORT
• UART
• FIR
• IIR
All the SSLDD 2.0 modules which have compatibility with SSLDD 3.0 will be deprecated in future release for ADSP-SC58x and ADSP-SC57x processors.