Question:
Support for eclipse plugins in CCES
Answer:
CrossCore Embedded Studio (CCES) is based on the Eclipse Platform and uses many features such as the C/C++ Development Tooling (CDT). We also build on a particular version of the Platform and include a particular version of the CDT etc.
CCES does not come bundled with many of the Eclipse features that other 3rd party features and plugins require as a dependency.
Having said the above, if a 3rd party feature or plugin requires a dependency and that dependency is available with CCES or can be installed into CCES (i.e. its dependencies can be resolved), then it is more than possible to install many 3rd party features and plugins.
We are not aware of any changes to CCES that will interfere with the operation of 3rd party features or plugins.