Question:
How to generate two interrupts on Rising and Falling edge of same single input pin using two PINT modules in single core?
Answer:
The attached example for ADSP-BF609 EZKIT using SSLDD will help to understand how to configure interrupts on both edges of same single input pin using two different PINT modules in single core. Here single input source is Push button 1 in EZKit