Revolutionizing Flow Cytometry: 20-Bit Precision Signal Chain

    In this webinar, we will reassess the design of electronics for Flow Cytometry applications. In the past, 20-bit, 40 MSPS analog-to-digital converters...
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
    • COTS SoMs & Phased Array Solutions for Rapid RF Subsystem Integration
    • LEO Satcom: Application of RF, Mixed-Signal, & Beamforming ICs
    • 3 Real World Methods to Make Your Power Supply More Intelligent
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC's Quiz AQQ300 about Divisibility by 6

      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Taming the AI Power Storm: Part 2 of 3 Test your...
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
    Clock Tree Design and Why “PLL Locked” Is Not Enough

    In high-performance RF systems, clocking architecture is a foundational element that directly governs signal integrity, synchronization, and overall system...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Improving Industrial Functional Safety Compliance with High Performance Supervisory CircuitsPart 5: Sequencers Eliminate Systematic Failures

    This article shifts focus from managing the quantitative metrics of functional safety toward mastering the qualitative yet equally critical challenge:...

EngineerZone
EngineerZone
CrossCore Embedded Studio and Add-ins
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
CrossCore Embedded Studio and Add-ins
  • Processors & DSP
  • Software & Development Tools
  • CrossCore Embedded Studio and Add-ins
  • Cancel
CrossCore Embedded Studio and Add-ins
Documents UART DMA mode operation in SC58x processors Audit
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • FAQ
  • +a.b silicon into a x.y silicon target: FAQ
  • +accel_xxxx: FAQ
  • +ADC & DAC in audio application: FAQ
  • Add submodule files in CCES
  • +Add version of application in loader file: FAQ
  • Add-in license: FAQ
  • +ADI_SPI_TRANSCEIVER: FAQ
  • +adi_spu_Init() API: FAQ
  • +ADSO-BF609 EZkit: FAQ
  • +ADSP-21364: FAQ
  • +ADSP-214xx: FAQ
  • +ADSP-21569 Ez-kit: FAQ
  • +ADSP-21569: FAQ
  • +ADSP-2183x:FAQ
  • +ADSP-BF609 EZKIT: FAQ
  • +ADSP-BF609: FAQ
  • +ADSP-BF707: FAQ
  • +ADSP-BF70x: FAQ
  • +ADSP-SC589: FAQ
  • -ADSP-SC58x: FAQ
    • Configure CODEC using TWI
    • FreeRTOS MCAPI example for SC584
    • Link Port DMA using SSLDD3.0 Audit
    • Linkport Trigger Master code for SC584 Audit
    • MemmappedRead Example code for SC584
    • RTL-Level SEC Handler with a Timer
    • Sample based code for I2S mode using 3.0APIs Audit
    • Sample based code for TDM4 mode using 3.0APIs
    • Software triggering interrupt in ADSP-SC58x/2158x Evaluation boards Audit
    • UART DMA mode operation in SC58x processors Audit
    • UART Sample application codes for SC5xx processors Audit
    • What is the difference between ADSP-SC58x and ADSP-214xx processors while using run time library functions which access data from external memory? Audit
  • +ADSP-SC59x: FAQs
  • +ADSP-SC5xx: FAQ
  • +ADSP-SC8xx FAQs
  • +ADSP21489: FAQ
  • +ADSP215xx: FAQ
  • +alignment pragma: FAQ
  • +ARM CORE: FAQ
  • +ARM to Sharc: FAQ
  • +avoid when a project is getting build: FAQ
  • +BF-609 Evaluation board: FAQ
  • +BF518 Processor: FAQ
  • +BF703: FAQ
  • +BF706 EZ-KIT: FAQ
  • +BF706: FAQ
  • +BF706mini BSP project: FAQ
  • +BF707 SPI: FAQ
  • BITEXP and BITRET for ADSP-214xx
  • C and C++ standard library in CCES?
  • +C source file: FAQ
  • +C++ code: FAQ
  • +C-code ISRs: FAQ
  • cache invalidation and cache flushing
  • +Callback function: FAQ
  • +Calling Library Functions: FAQ
  • +cc1138: FAQ
  • +CCES: FAQ's
  • +cldp: FAQ
  • Clip double precision floating-point in C Audit
  • +CLKIN: FAQ
  • +Code folding in CCES: FAQ
  • +Configuring the Loader, Linker and Archiver: FAQ
  • +connect to the Blackfin: FAQ
  • Create Library files for individual modules Audit
  • Creating and Linking a .dlb in CCES
  • +CrossCore Embedded Studio STDIO: FAQ
  • +CROSSCORE: FAQ
  • Custom debug configurations in CCES
  • +Data Member Alignment: FAQ
  • +Device Driver programming: FAQ
  • Difference between ADZS-HPUSB and ADZS-USB ICE Audit Audit
  • Difference between Debug and Release configurations
  • +Difference between Emulator and Simulator: FAQ
  • +disable prelinker: FAQ
  • DND mode in CCES
  • Does CCES have any API that can be used to build automation test platform with Python Audit
  • Does ICE-1000 supported ADSP-CM407F? Audit
  • +Driver example for Timer windowed watchdog period mode.
  • +Embedded applications: FAQ
  • +EV-21569-SOM: FAQ
  • Example code for SPORT slave trigger in ADSP-21569 Ezkit Audit Audit
  • Export console output to the desired file Audit
  • export/import CCES preferences settings
  • +EXTCLK_MODE: FAQ
  • Flash Programmer Drivers for ADSP-2183x/SC83x and ADSP-SC5xx ARM Cortex A5 Cores
  • GUL-XP board with EZkit license Audit
  • +How to access darkmode appearance in CCES?
  • +How to access stereo channels individually in the Audio_Passthrough_I2S example present in GUL BSP?
  • +How to avoid CORE0 and DEBUG: FAQ
  • How to build a specific code from single source file for a specific core?
  • +How to convert long double into string: FAQ
  • How to create library files for individual modules? Audit
  • +how to deassert Slave: FAQ
  • +How to do profiling: FAQ
  • How to obtain PCB library files for ADI processors Audit
  • How to pass arguments from command line in CCES runner
  • +How to protect shared code/ data: FAQ
  • How To remove automatically added "includes" folders in CCES project Audit
  • How to use "log10f_simd" Audit
  • How to use commands in CCES runner Audit
  • How to use Device programmer in EVAL-ADICUP360 board Audit
  • How to use optimized libraries for FFT Audit
  • +HW Accelerator and SW libraries: FAQ
  • INPUT SECTIONS & INPUT SECTIONS PIN EXCLUSIVE Audit
  • Interrupt header files along with -char-size-32 switch in Sharc Audit
  • +Interrupt Vector Table: FAQ
  • Is it possible to perform stepping into the code in CCES Runner. Audit
  • Is there a way to list symbols from library (*.dlb) file? Audit
  • Is there a way to mangle or remove internal symbols ? Audit
  • JTAG switch Interface for EV-SOMCRR-EZLITE and EV-SOMCRR-EZKIT: Audit
  • +LDF from C code: FAQ
  • +linker map file: FAQ
  • +List of Processors: FAQ
  • +Loader File: FAQ
  • +MCAPI package: FAQ
  • +node-locked license: FAQ
  • +non-blocking peek functions: FAQ
  • Optimization in ARM Audit
  • +PART_SPECIFIC_HEADERS: FAQ
  • +path variables: FAQ
  • +peripheral Error: FAQ
  • +PINT modules: FAQ
  • +PM bus: FAQ
  • +Project Explorer tree: FAQ
  • +PWM mode: FAQ
  • +quad SPI mode: FAQ
  • Reset SHARC core from ARM core using RCU in SC573 Audit
  • +RTOS for older Blackfin or older SHARC: FAQ
  • +SC-573 EZkit: FAQ
  • +SC83x-FAQ
  • +SDRAM: FAQ
  • +SHARC 21469: FAQ
  • +SHARC0: FAQ
  • +SHARC: FAQ
  • +sharing global data between cores: FAQ
  • +SigmaStudioForSHARC: FAQ
  • +SIMD code: FAQ
  • +SIMD: FAQ
  • sizeof() built-in function in BF and Sharc processors Audit
  • +SPI core mode with callback: FAQ
  • +SPI flash: FAQ
  • +SPORT API: FAQ
  • +SPORT: FAQ
  • +SRCU bit: FAQ
  • SRU and DAI routing via GUI
  • +SSLDD 2.0 and SSLDD 3.0: FAQ
  • +SSLDD 3.0: FAQ
  • +SSLDD3.0: FAQ
  • +stack overflow: FAQ
  • +Static library & IP protection: FAQ
  • Streaming Data input and output in CCES
  • +suppress assembler preprocessor warning: FAQ
  • SWD with ICE-1000
  • +system.svc: FAQ
  • TDM with both SPORT channels Audit
  • TWI Transfer using 3.0 APIs
  • +two PINT modules: FAQ
  • +TX and RX DMA Interrupts: FAQ
  • Types of Pragma usage Audit
  • +U-Law and A-Law: FAQ
  • +UART Device Driver: FAQ
  • +UART ISR Callback: FAQ
  • UART sample driver code for BF706mini Audit
  • +VisualDSP++: FAQ
  • +Wakeup processor from Hibernate: FAQ
  • +When callback occurs: FAQ
  • +word addressable program: FAQ
  • [FAQ] : FORCE CONTIGUITY Audit
  • “Peripherals view” in CCES

UART DMA mode operation in SC58x processors Audit

Question:

Example project which helps to understand UART DMA operation in SC58x processors

Answer:

The attached project which helps to understand UART DMA mode in a loop back manner. Here we used UART0 for transmitting and receiving ten Integer data

UART_DMA.zip

  • Share
  • History
  • More
  • Cancel
 
Related Content
  • RE: UART DMA issue
    Mr.Kristrnsen
    Thanks
  • UART DMA
    Sandra
    Hi, I'm using BF537 and want to use UART DMA for transmission and leave the Rx interrupt based. Can the UART DMA driver work in this setup? Thanks. Best Regards, Sandra
  • RE: BF514F UART RX DMA Problem
    ADIApproved
    Hi Connor, We would suggest you to refer the FAQ which talks about "Example project which helps to understand UART DMA mode operation in SC58x processors" and example code available in the below mentioned...
 
Related Content
  • RE: UART DMA issue
    Mr.Kristrnsen
    Thanks
  • UART DMA
    Sandra
    Hi, I'm using BF537 and want to use UART DMA for transmission and leave the Rx interrupt based. Can the UART DMA driver work in this setup? Thanks. Best Regards, Sandra
  • RE: BF514F UART RX DMA Problem
    ADIApproved
    Hi Connor, We would suggest you to refer the FAQ which talks about "Example project which helps to understand UART DMA mode operation in SC58x processors" and example code available in the below mentioned...