Post Go back to editing

Exporting makefile and building from the command line

Thread Summary

The user asked if CCES can export a single makefile or if it can be invoked from the command line to build a project. The final answer indicates that while CCES does not support exporting a single makefile, it can be built from the command line using the ccesc.exe tool with specific options for workspace and project locations and build configuration.
AI Generated Content

Is there a way in CCES to export a single makefile similar to VisualDSP's Project:Export Makefile that allows for building to any target from the command line?

Or is there a way to invoke CCES from the command line to build the project without launching the IDE?

Thanks,

Nick