Post Go back to editing

Exporting makefile and building from the command line

Thread Summary

The user asked if CCES can export a single makefile or if it can be invoked from the command line to build a project. The final answer indicates that while CCES does not support exporting a single makefile, it can be built from the command line using the ccesc.exe tool with specific options for workspace and project locations and build configuration.
AI Generated Content

Is there a way in CCES to export a single makefile similar to VisualDSP's Project:Export Makefile that allows for building to any target from the command line?

Or is there a way to invoke CCES from the command line to build the project without launching the IDE?

Thanks,

Nick

  • Hi, Nick

    CCES does not have a way to export a single makefile but it provides a way to build projects from the command line. Assume you installed CCES at the default location. Here is an example of the command:

    C:\Analog Devices\CrossCore Embedded Studio 1.0.1\Eclipse\ccesc.exe -nosplash -consoleLog -application com.analog.crosscore.headlesstools -data "C:/workspace"

    -project "C:/yourprojectlocation" -build Debug

    The option -data indicates the local location of your workspace. The option -project indicates the local location of your project. The option -build indicates the build configuration.

    Cesar

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.