Post Go back to editing

Error -- No processor information found

I have a CCES 21469 project that is giving me this error message

Loading application: "E:\Research\uTTCOS_Backups\VDSP2013_TTCOSLibraryBuild\ADSP21469Specific\SHARC21469_uTTCOS2013_LibBuilder\Debug\SHARC21469_uTTCOS2013_LibBuilder.dxe"

No processor information found; assuming ADSP-21469.

Load complete.

The board has existing code that flashes the LEDS -- when I download the code -- the flash temporarily stops -- indicating that something is happening over the emulator -- but then the flashing restarts

I have break points in the code -- but they don't get reached -- indicating to me that the code is not really running.

I can download other projects to the boaard -- no problems

I have cleaned rebuilt, rebooted HPUSB-ICE and board and then the whole system

I can force the project to ask me about hooking up to the board -- select processor and emulator

I even went and changed the main to be this

#include <stdio.h>

void main(void) {

    printf("Hi there\n");

}

No luck.

This was an imported original VDSP project -- so I think I will just delete the CCES port directories -- reboot the system and reconvert it

However, before I do that -- anything you would like me to examine

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.