Is it possible to have VDSP AND CrossCore setup on the same PC

Hi,

I would like to know if there is a way to setup VDSP and CrossCore on the same development PC ?

For now I tried and the result is a real disaster as my original VDSP setup is broken, all DXE can be load but after if I start them, the execution is stuck !

Any idea to, restore the VDSP setup (I already reinstall it without success) and/or the run both IDE on the same PC will be welcome.

Alex

Parents
  • Hi in fact I was able to make some progress .... And based on that I can give some fact & advice

    - porting VDSP code to CCES may require some code change (in my case mainly for interrupt management/registration)

    - generated lib are compatible

    - I was able to share the same code base (or working copy)

         - I used a #ifdef _CCES_ to customized my src code for CCES or VDSP

         - For VDSP I used to group all the build artifcat in an only one build folder (and the same for the intermediate), and      I was able to do the same with the CCES project so that I can automate the VDSP and CCES build and get        their different build artifact

    Hoping it can help.

Reply
  • Hi in fact I was able to make some progress .... And based on that I can give some fact & advice

    - porting VDSP code to CCES may require some code change (in my case mainly for interrupt management/registration)

    - generated lib are compatible

    - I was able to share the same code base (or working copy)

         - I used a #ifdef _CCES_ to customized my src code for CCES or VDSP

         - For VDSP I used to group all the build artifcat in an only one build folder (and the same for the intermediate), and      I was able to do the same with the CCES project so that I can automate the VDSP and CCES build and get        their different build artifact

    Hoping it can help.

Children
No Data