Post Go back to editing

CCES 2.3.0 crash using Sigma Studio 3.7.0 for SHARC example

My setup is:

  •  SC589 eval board BOM rev 1.6, 589 rev 1-0.1, switches and jumpers as per the guide.
         with ICE 1000 rev 1.1
  • USB2Z rev 1.3
  • being used from SigmaStudio 3.12 build 4 (though probably not relevant to the problem)
  • CCES 2.3.0,
  • SS for Sharc 3.7.0.
  • My development system is Windows 7 with the latest patches.

I previously experienced this same exact problem and thought it was "solved" by uninstalling/reinstalling CCES, but it has come back on its own so there must be a more fundamental problem. The steps are described in the ADI document: \SoftwareModules\SigmaStudioForSHARC-SH-Rel3.7.0\Docs\AE_03_SS4G_QuickStartGuide.pdf

The workspace I'm using in the attached previously worked. After opening the workspace, selecting Debug will cause CCES to crash while updating the Debug dialog box. The console window indicates that all 3 .dxe loaded successfully and then CCES crashes within a second of that. There are no dialogs or other error reports. I have attached the crash dump as well.

I did not try reinstalling again since that's kind of a painful solution, and maybe it was coincidental that the problem went away when I did that last time.

attachments.zip